If a GangLoadParameters function is used using GANG430.dll of a version 1.01.07, the following phenomenon will occur.
1. An unnecessary F_ERASE_PINFO and F_ERASE_CHECK_PINFO flag is set up when the following setup is performed to lFlags of an argument.
(F_ELASE_INFO | F_ERASE_MAIN | F_PROGRAM_MASS | F_ERASE_CHECK_INFO | F_ERASE_CHECK_MAIN | F_VERIFY)
I checked on the screen of MSP-GANG Programmer after function execution.
2. As a result, if a GangMainProcess function is fail, and GangGetResult function is return "Error 58 Verify Error".
3. This does not occur, after execute the GangLoadParameters function which set up the lFlags (F_ERASE_MASS | F_PROGRAM_MASS | F_ERASE_CHECK_MASS | F_VERIFY) also at once.
In addition, this occurred, even if it used the same setup by the sample program "CPP_Wrapper_demo".
There is no telling how carry out and this error comes out.
Aren't there those who understand a cause?