I am using a MSP4305529 to collect data from an encoder and display it on an LCD. I am also saving the data and am able to send it to Hyper Terminal for viewing. All of that works fine but I would like to be able to eliminate the PC and send the data directly from the 5529 to a generic HP inkjet printer. I could send it to a POS printer (Seiko) but would like to be able to connect the USB cable from the 5529 to the printer and send data for printing. I am using Energia to generate the downloaded code.
The problem as I see it is that the HP printer is not setup to receive the serial data that is being transmitted. I guess in effect, I need a driver so that the printer thinks it is being driven by a PC.
I am a retired Mechanical Engineer and have been using computers since the early 1960's when I first started using BASIC on a GE Timeshare terminal (ten characters a second). I am not proficient in C but have learned enough to use Energia.
Any help or thought would be greatly appreciated.