Hello ....
I have used an example SPI example MSP-FET430P140 Demo - USART0, SPI 3-Wire Master. This example does not work for me. In this example the UTXIFG0-flag (TXBUF0, Register IFG1) is teste in an Interrupt. If I do that a hungup is the result.
I have found a better way, when I test the UTXIFG0-flag outside the Interrupt and I disable the UTXIFG0-Interrupt in an Interrupt. When the buffer is empty, the UTXIFG0-flag goes high and the UTXIFG0 interrupt can be enabled.
Regards Jürgen Rieger