Hi.
I'm being forced by a client to make RTC backup voltage (AUXVCC3) on MSP430F6732 same as VCC (3.3V). I may have to end up adding an expensive ultracap just to make the voltage same!
He thinks that if I use a CR2032 battery (3V), the oscillator will lose its precision while switching from 3.3V to 3V on power failure! I think the crystal runs on 1V generated internally and would continue to provide precise ticks irrespective of the change in input voltage.
And, of course, the precision in timing would remain the same irrespective of whether the source is 3.3V or 3V!
Am I correct in this understanding or is he right?
Thanks,
Anup