This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5338 and Field software upgrade on GPRS network (OTA).

Other Parts Discussed in Thread: MSP430F5338

Hi,

Hardware : MSP430F5338 with GSM/GPRS modem with ftp and TCP/IP stack.

Software and IDE : TI-RTOS, CCS5.5. Approximate image size 110-120K.

Requirement : Send TI.TXT from server to the MSP430F5338 target on GPRS network, parse if needed on target and write to flash.

Help/Clarification Required :

1. Is the TI.TXT file is flash image so that I can write file data directly at specified address (@) ? or it is text (ASCII) and need any conversion before flashing into flash ?

2. If TI.TXT file is in text (ASCII) any other format, is there any parser available in "C" ? I can run the parser on target and flash.

3. Any one used GPRS network for firmware upgrade. Which file format and parser used ?

Appreciate your help.

Thanks,

CB Kolar

**Attention** This is a public forum