Reference: http://e2e.ti.com/support/microcontrollers/msp430/f/166/t/19726.aspx
If I read these posts correctly, I think that there is added delay between the "Port select XT1" and "Switch XT1 On" to allow the oscillator to stabilize before using, correct?
On the F5529, the XT1 is defaulted to "on" on powerup. Does that mean it should be turned off, then allowed to stablize, then turned on?
I also need to set up XCAP to be different that default. So, should I
1. Turn off XT1.
2. Port select Xt1.
3. Wait for stabilization.
4. Turn on XT1.
5. Then route to RTC, ACLK and any other place it is being used