Hi,
I have acquired a couple of ADS1118 BoosterPacks http://www.ti.com/tool/430boost-ads1118?keyMatch=ADS1118&tisearch=Search-EN with an intention to use them in a lab without any extra job on fixing them.
Unfortunately the contrast on LCDs is very bad (the background dots, which should not be on are too dark)
Now I need to study the LCD specification and the controller specification to fix it (if possible).
My feedback is: That nice would be much better with a LCD contrast set properly.
And the question is: Can someone save me time and give a hint what settings to change?
I see within the LCD_init() function the following lines:
LCD_writecom(0x56); //power control
LCD_writecom(0x6D); //follower control
LCD_writecom(0x70); //contrast
Thanks
Jan