Hi
we are designed a product to interface a 2GB SD card to msp430FR5969 but now 2GB is EOL so can i directly replace 2 GB with 8 GB or anything i need to consider in replacing 2GB to 8GB card.
Regards
Nandish
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
we are designed a product to interface a 2GB SD card to msp430FR5969 but now 2GB is EOL so can i directly replace 2 GB with 8 GB or anything i need to consider in replacing 2GB to 8GB card.
Regards
Nandish
Hi Nadhish,
My advise is
1. You should have to interface the MMC (if you can get one) card before SD card.
2. other wise interface SD card less than 2 GB requires some more CMD commands then MMC.
3. Above 2GB (4gb , 8gb )there are more & complex CMD ( APCMD = 0X80+CMD ) commands are required.
4. thus first interface 2GB card (if not mmc) and then make some changes and interface card above 2GB
Good Luck.
Regards,
Dharmendra Sharma
INDIA
________________________________________
Do, click "Verify Answer", if any of my replies helps solve your problem.
Hi All,
I will have to interface an SD card with MSP430FR5969 soon as well. Did you guys write your own code or did you use a library such as FatFS or PetitFat?
Thanks,
Nipun
Nipun,
if you really wanna learn how SD works... and all its internal architecture then
follow the tutorial link..
http://codeandlife.com/2012/04/02/simple-fat-and-sd-tutorial-part-1/
Regards,
Dharmendra Sharma
INDIA
__________________________________
Do, click "Verify Answer", if any of my replies helps solve your problem.
Dharmendra,
Thank you very much for the link, I will take a look at it!
- Nipun
SD cards above 4GB (HC standard) do not always support the MMC-compatible serial protocol. Some don’t. Also, like micro-SD below 4GB, they often do not support the MMC entry sequence and require the (slightly different) SD card sequence. (standard SD cards in standard or mini size support both).
Also, SDHC cards have a different interpretation of some of the information sector data (regarding capacity and block sizes), require asking for the supply voltage info register, and their read and write commands do not take a linear address, but a sector address (address parameter is not bit 0..31 but rather 9..41)
You can download the complete specifications from SanDisk.
**Attention** This is a public forum