All:
F5528 - if I force an XT1 fault (by shorting the crystal, I get the XT1LFOFFG bit on in the UCSCTL7 register - at which point, the oscillator is forced to REFO, confirmed by observing ACLK on P1.0 - however, I would also expect the SELA bits to change, showing that REFO is now being used rather than XT1. Is this expected behavior?