HI
I proceed to some modification to write in SDcard , i will share my code hoping someone can help me.
I connect the msp430g2553, with a sdcard and a LCD, he can mount the card and recognize the disk, but do not write in the file.
#include <msp430.h> #include <stdint.h> #include "spi.h" #ifndef __MSP430_HAS_USCI__ #error "Error! This MCU doesn't have a USCI peripheral" #endif #define SPI_MODE_0 UCCKPH | UCMSB| UCMST | UCSYNC /* CPOL=0 CPHA=0 */ #define SPI_MODE_3 UCCKPL | UCMSB| UCMST | UCSYNC /* CPOL=1 CPHA=1 */ /** * spi_initialize() - Initialize and enable the SPI module * * P2.0 - CS (active low) * P1.5 - SCLK * P1.6 - SIMO * P1.7 - MOSI * */ void spi_initialize(void) { UCB0CTL1 = UCSSEL_2 | UCSWRST; // source USCI clock from SMCLK, put USCI in reset mode UCB0CTL0 |= SPI_MODE_0; // SPI MODE 0 - CPOL=0 CPHA=0 // note: UCCKPH is inverted from CPHA P1SEL |= BIT5 | BIT6 | BIT7; // configure P1.5, P1.6, P1.7 for USCI P1SEL2 |= BIT5 | BIT6 | BIT7; UCB0BR0 = LOBYTE(SPI_400kHz); // set initial speed 16MHz/400000 = 400kHz UCB0BR1 = HIBYTE(SPI_400kHz); P2OUT |= BIT0; // CS on P2.0. start out disabled P2DIR |= BIT0; // CS configured as output UCB0CTL1 &= ~UCSWRST; // release for operation } /** * spi_send() - send a byte and recv response */ uint8_t spi_send(const uint8_t c) { while (!(UC0IFG & UCB0TXIFG)) ; // wait for previous tx to complete UCB0TXBUF = c; // setting TXBUF clears the TXIFG flag while (!(UC0IFG & UCB0RXIFG)) ; // wait for an rx character? return UCB0RXBUF; // reading clears RXIFG flag } /** * spi_receive() - send dummy btye then recv response */ uint8_t spi_receive(void) { while (!(UC0IFG & UCB0TXIFG)) ; // wait for any previous xmits to complete UCB0TXBUF = 0xFF; // Send dummy packet to get data back. while (!(UC0IFG & UCB0RXIFG)) ; // wait to recv a character? return UCB0RXBUF; // reading clears RXIFG flag } /** * spi_setspeed() - set new clock divider for USCI * * USCI speed is based on the SMCLK divided by BR0 and BR1 * initially we start slow (400kHz) to conform to SDCard * specifications then we speed up once initialized (16Mhz) * */ void spi_set_divisor(const uint16_t clkdiv) { UCB0CTL1 |= UCSWRST; // go into reset state UCB0BR0 = LOBYTE(clkdiv); UCB0BR1 = HIBYTE(clkdiv); UCB0CTL1 &= ~UCSWRST; // release for operation }
/*----------------------------------------------------------------------------/ / Petit FatFs - FAT file system module R0.02a (C)ChaN, 2010 /-----------------------------------------------------------------------------/ / Petit FatFs module is an open source software to implement FAT file system to / small embedded systems. This is a free software and is opened for education, / research and commercial developments under license policy of following trems. / / Copyright (C) 2010, ChaN, all right reserved. / / * The Petit FatFs module is a free software and there is NO WARRANTY. / * No restriction on use. You can use, modify and redistribute it for / personal, non-profit or commercial use UNDER YOUR RESPONSIBILITY. / * Redistributions of source code must retain the above copyright notice. / /-----------------------------------------------------------------------------/ / Jun 15,'09 R0.01a First release. (Branched from FatFs R0.07b.) / / Dec 14,'09 R0.02 Added multiple code page support. / Added write funciton. / Changed stream read mode interface. / Dec 07,'10 R0.02a Added some configuration options. / Fixed fails to open objects with DBCS character. /----------------------------------------------------------------------------*/ #include "pff.h" /* Petit FatFs configurations and declarations */ #include "diskio.h" /* Declarations of low level disk I/O functions */ /*-------------------------------------------------------------------------- Module Private Definitions ---------------------------------------------------------------------------*/ #if _FS_FAT32 #define LD_CLUST(dir) (((DWORD)LD_WORD(dir+DIR_FstClusHI)<<16) | LD_WORD(dir+DIR_FstClusLO)) #else #define LD_CLUST(dir) LD_WORD(dir+DIR_FstClusLO) #endif /*--------------------------------------------------------*/ /* DBCS code ranges and SBCS extend char conversion table */ #if _CODE_PAGE == 932 /* Japanese Shift-JIS */ #define _DF1S 0x81 /* DBC 1st byte range 1 start */ #define _DF1E 0x9F /* DBC 1st byte range 1 end */ #define _DF2S 0xE0 /* DBC 1st byte range 2 start */ #define _DF2E 0xFC /* DBC 1st byte range 2 end */ #define _DS1S 0x40 /* DBC 2nd byte range 1 start */ #define _DS1E 0x7E /* DBC 2nd byte range 1 end */ #define _DS2S 0x80 /* DBC 2nd byte range 2 start */ #define _DS2E 0xFC /* DBC 2nd byte range 2 end */ #elif _CODE_PAGE == 936 /* Simplified Chinese GBK */ #define _DF1S 0x81 #define _DF1E 0xFE #define _DS1S 0x40 #define _DS1E 0x7E #define _DS2S 0x80 #define _DS2E 0xFE #elif _CODE_PAGE == 949 /* Korean */ #define _DF1S 0x81 #define _DF1E 0xFE #define _DS1S 0x41 #define _DS1E 0x5A #define _DS2S 0x61 #define _DS2E 0x7A #define _DS3S 0x81 #define _DS3E 0xFE #elif _CODE_PAGE == 950 /* Traditional Chinese Big5 */ #define _DF1S 0x81 #define _DF1E 0xFE #define _DS1S 0x40 #define _DS1E 0x7E #define _DS2S 0xA1 #define _DS2E 0xFE #elif _CODE_PAGE == 437 /* U.S. (OEM) */ #define _DF1S 0 #define _EXCVT {0x80,0x9A,0x90,0x41,0x8E,0x41,0x8F,0x80,0x45,0x45,0x45,0x49,0x49,0x49,0x8E,0x8F,0x90,0x92,0x92,0x4F,0x99,0x4F,0x55,0x55,0x59,0x99,0x9A,0x9B,0x9C,0x9D,0x9E,0x9F, \ 0x41,0x49,0x4F,0x55,0xA5,0xA5,0xA6,0xA7,0xA8,0xA9,0xAA,0xAB,0xAC,0x21,0xAE,0xAF,0xB0,0xB1,0xB2,0xB3,0xB4,0xB5,0xB6,0xB7,0xB8,0xB9,0xBA,0xBB,0xBC,0xBD,0xBE,0xBF, \ 0xC0,0xC1,0xC2,0xC3,0xC4,0xC5,0xC6,0xC7,0xC8,0xC9,0xCA,0xCB,0xCC,0xCD,0xCE,0xCF,0xD0,0xD1,0xD2,0xD3,0xD4,0xD5,0xD6,0xD7,0xD8,0xD9,0xDA,0xDB,0xDC,0xDD,0xDE,0xDF, \ 0xE0,0xE1,0xE2,0xE3,0xE4,0xE5,0xE6,0xE7,0xE8,0xE9,0xEA,0xEB,0xEC,0xED,0xEE,0xEF,0xF0,0xF1,0xF2,0xF3,0xF4,0xF5,0xF6,0xF7,0xF8,0xF9,0xFA,0xFB,0xFC,0xFD,0xFE,0xFF} #elif _CODE_PAGE == 720 /* Arabic (OEM) */ #define _DF1S 0 #define _EXCVT {0x80,0x81,0x45,0x41,0x84,0x41,0x86,0x43,0x45,0x45,0x45,0x49,0x49,0x8D,0x8E,0x8F,0x90,0x92,0x92,0x93,0x94,0x95,0x49,0x49,0x98,0x99,0x9A,0x9B,0x9C,0x9D,0x9E,0x9F, \ 0xA0,0xA1,0xA2,0xA3,0xA4,0xA5,0xA6,0xA7,0xA8,0xA9,0xAA,0xAB,0xAC,0xAD,0xAE,0xAF,0xB0,0xB1,0xB2,0xB3,0xB4,0xB5,0xB6,0xB7,0xB8,0xB9,0xBA,0xBB,0xBC,0xBD,0xBE,0xBF, \ 0xC0,0xC1,0xC2,0xC3,0xC4,0xC5,0xC6,0xC7,0xC8,0xC9,0xCA,0xCB,0xCC,0xCD,0xCE,0xCF,0xD0,0xD1,0xD2,0xD3,0xD4,0xD5,0xD6,0xD7,0xD8,0xD9,0xDA,0xDB,0xDC,0xDD,0xDE,0xDF, \ 0xE0,0xE1,0xE2,0xE3,0xE4,0xE5,0xE6,0xE7,0xE8,0xE9,0xEA,0xEB,0xEC,0xED,0xEE,0xEF,0xF0,0xF1,0xF2,0xF3,0xF4,0xF5,0xF6,0xF7,0xF8,0xF9,0xFA,0xFB,0xFC,0xFD,0xFE,0xFF} #elif _CODE_PAGE == 737 /* Greek (OEM) */ #define _DF1S 0 #define _EXCVT {0x80,0x81,0x82,0x83,0x84,0x85,0x86,0x87,0x88,0x89,0x8A,0x8B,0x8C,0x8D,0x8E,0x8F,0x90,0x92,0x92,0x93,0x94,0x95,0x96,0x97,0x80,0x81,0x82,0x83,0x84,0x85,0x86,0x87, \ 0x88,0x89,0x8A,0x8B,0x8C,0x8D,0x8E,0x8F,0x90,0x91,0xAA,0x92,0x93,0x94,0x95,0x96,0xB0,0xB1,0xB2,0xB3,0xB4,0xB5,0xB6,0xB7,0xB8,0xB9,0xBA,0xBB,0xBC,0xBD,0xBE,0xBF, \ 0xC0,0xC1,0xC2,0xC3,0xC4,0xC5,0xC6,0xC7,0xC8,0xC9,0xCA,0xCB,0xCC,0xCD,0xCE,0xCF,0xD0,0xD1,0xD2,0xD3,0xD4,0xD5,0xD6,0xD7,0xD8,0xD9,0xDA,0xDB,0xDC,0xDD,0xDE,0xDF, \ 0x97,0xEA,0xEB,0xEC,0xE4,0xED,0xEE,0xE7,0xE8,0xF1,0xEA,0xEB,0xEC,0xED,0xEE,0xEF,0xF0,0xF1,0xF2,0xF3,0xF4,0xF5,0xF6,0xF7,0xF8,0xF9,0xFA,0xFB,0xFC,0xFD,0xFE,0xFF} #elif _CODE_PAGE == 775 /* Baltic (OEM) */ #define _DF1S 0 #define _EXCVT {0x80,0x9A,0x91,0xA0,0x8E,0x95,0x8F,0x80,0xAD,0xED,0x8A,0x8A,0xA1,0x8D,0x8E,0x8F,0x90,0x92,0x92,0xE2,0x99,0x95,0x96,0x97,0x97,0x99,0x9A,0x9D,0x9C,0x9D,0x9E,0x9F, \ 0xA0,0xA1,0xE0,0xA3,0xA3,0xA5,0xA6,0xA7,0xA8,0xA9,0xAA,0xAB,0xAC,0xAD,0xAE,0xAF,0xB0,0xB1,0xB2,0xB3,0xB4,0xB5,0xB6,0xB7,0xB8,0xB9,0xBA,0xBB,0xBC,0xBD,0xBE,0xBF, \ 0xC0,0xC1,0xC2,0xC3,0xC4,0xC5,0xC6,0xC7,0xC8,0xC9,0xCA,0xCB,0xCC,0xCD,0xCE,0xCF,0xB5,0xB6,0xB7,0xB8,0xBD,0xBE,0xC6,0xC7,0xA5,0xD9,0xDA,0xDB,0xDC,0xDD,0xDE,0xDF, \ 0xE0,0xE1,0xE2,0xE3,0xE5,0xE5,0xE6,0xE3,0xE8,0xE8,0xEA,0xEA,0xEE,0xED,0xEE,0xEF,0xF0,0xF1,0xF2,0xF3,0xF4,0xF5,0xF6,0xF7,0xF8,0xF9,0xFA,0xFB,0xFC,0xFD,0xFE,0xFF} #elif _CODE_PAGE == 850 /* Multilingual Latin 1 (OEM) */ #define _DF1S 0 #define _EXCVT {0x80,0x9A,0x90,0xB6,0x8E,0xB7,0x8F,0x80,0xD2,0xD3,0xD4,0xD8,0xD7,0xDE,0x8E,0x8F,0x90,0x92,0x92,0xE2,0x99,0xE3,0xEA,0xEB,0x59,0x99,0x9A,0x9D,0x9C,0x9D,0x9E,0x9F, \ 0xB5,0xD6,0xE0,0xE9,0xA5,0xA5,0xA6,0xA7,0xA8,0xA9,0xAA,0xAB,0xAC,0x21,0xAE,0xAF,0xB0,0xB1,0xB2,0xB3,0xB4,0xB5,0xB6,0xB7,0xB8,0xB9,0xBA,0xBB,0xBC,0xBD,0xBE,0xBF, \ 0xC0,0xC1,0xC2,0xC3,0xC4,0xC5,0xC7,0xC7,0xC8,0xC9,0xCA,0xCB,0xCC,0xCD,0xCE,0xCF,0xD0,0xD1,0xD2,0xD3,0xD4,0xD5,0xD6,0xD7,0xD8,0xD9,0xDA,0xDB,0xDC,0xDD,0xDE,0xDF, \ 0xE0,0xE1,0xE2,0xE3,0xE5,0xE5,0xE6,0xE7,0xE7,0xE9,0xEA,0xEB,0xED,0xED,0xEE,0xEF,0xF0,0xF1,0xF2,0xF3,0xF4,0xF5,0xF6,0xF7,0xF8,0xF9,0xFA,0xFB,0xFC,0xFD,0xFE,0xFF} #elif _CODE_PAGE == 852 /* Latin 2 (OEM) */ #define _DF1S 0 #define _EXCVT {0x80,0x9A,0x90,0xB6,0x8E,0xDE,0x8F,0x80,0x9D,0xD3,0x8A,0x8A,0xD7,0x8D,0x8E,0x8F,0x90,0x91,0x91,0xE2,0x99,0x95,0x95,0x97,0x97,0x99,0x9A,0x9B,0x9B,0x9D,0x9E,0x9F, \ 0xB5,0xD6,0xE0,0xE9,0xA4,0xA4,0xA6,0xA6,0xA8,0xA8,0xAA,0x8D,0xAC,0xB8,0xAE,0xAF,0xB0,0xB1,0xB2,0xB3,0xB4,0xB5,0xB6,0xB7,0xB8,0xB9,0xBA,0xBB,0xBC,0xBD,0xBD,0xBF, \ 0xC0,0xC1,0xC2,0xC3,0xC4,0xC5,0xC6,0xC6,0xC8,0xC9,0xCA,0xCB,0xCC,0xCD,0xCE,0xCF,0xD1,0xD1,0xD2,0xD3,0xD2,0xD5,0xD6,0xD7,0xB7,0xD9,0xDA,0xDB,0xDC,0xDD,0xDE,0xDF, \ 0xE0,0xE1,0xE2,0xE3,0xE3,0xD5,0xE6,0xE6,0xE8,0xE9,0xE8,0xEB,0xED,0xED,0xDD,0xEF,0xF0,0xF1,0xF2,0xF3,0xF4,0xF5,0xF6,0xF7,0xF8,0xF9,0xFA,0xEB,0xFC,0xFC,0xFE,0xFF} #elif _CODE_PAGE == 855 /* Cyrillic (OEM) */ #define _DF1S 0 #define _EXCVT {0x81,0x81,0x83,0x83,0x85,0x85,0x87,0x87,0x89,0x89,0x8B,0x8B,0x8D,0x8D,0x8F,0x8F,0x91,0x91,0x93,0x93,0x95,0x95,0x97,0x97,0x99,0x99,0x9B,0x9B,0x9D,0x9D,0x9F,0x9F, \ 0xA1,0xA1,0xA3,0xA3,0xA5,0xA5,0xA7,0xA7,0xA9,0xA9,0xAB,0xAB,0xAD,0xAD,0xAE,0xAF,0xB0,0xB1,0xB2,0xB3,0xB4,0xB6,0xB6,0xB8,0xB8,0xB9,0xBA,0xBB,0xBC,0xBE,0xBE,0xBF, \ 0xC0,0xC1,0xC2,0xC3,0xC4,0xC5,0xC7,0xC7,0xC8,0xC9,0xCA,0xCB,0xCC,0xCD,0xCE,0xCF,0xD1,0xD1,0xD3,0xD3,0xD5,0xD5,0xD7,0xD7,0xDD,0xD9,0xDA,0xDB,0xDC,0xDD,0xE0,0xDF, \ 0xE0,0xE2,0xE2,0xE4,0xE4,0xE6,0xE6,0xE8,0xE8,0xEA,0xEA,0xEC,0xEC,0xEE,0xEE,0xEF,0xF0,0xF2,0xF2,0xF4,0xF4,0xF6,0xF6,0xF8,0xF8,0xFA,0xFA,0xFC,0xFC,0xFD,0xFE,0xFF} #elif _CODE_PAGE == 857 /* Turkish (OEM) */ #define _DF1S 0 #define _EXCVT {0x80,0x9A,0x90,0xB6,0x8E,0xB7,0x8F,0x80,0xD2,0xD3,0xD4,0xD8,0xD7,0x98,0x8E,0x8F,0x90,0x92,0x92,0xE2,0x99,0xE3,0xEA,0xEB,0x98,0x99,0x9A,0x9D,0x9C,0x9D,0x9E,0x9E, \ 0xB5,0xD6,0xE0,0xE9,0xA5,0xA5,0xA6,0xA6,0xA8,0xA9,0xAA,0xAB,0xAC,0x21,0xAE,0xAF,0xB0,0xB1,0xB2,0xB3,0xB4,0xB5,0xB6,0xB7,0xB8,0xB9,0xBA,0xBB,0xBC,0xBD,0xBE,0xBF, \ 0xC0,0xC1,0xC2,0xC3,0xC4,0xC5,0xC7,0xC7,0xC8,0xC9,0xCA,0xCB,0xCC,0xCD,0xCE,0xCF,0xD0,0xD1,0xD2,0xD3,0xD4,0xD5,0xD6,0xD7,0xD8,0xD9,0xDA,0xDB,0xDC,0xDD,0xDE,0xDF, \ 0xE0,0xE1,0xE2,0xE3,0xE5,0xE5,0xE6,0xE7,0xE8,0xE9,0xEA,0xEB,0xDE,0x59,0xEE,0xEF,0xF0,0xF1,0xF2,0xF3,0xF4,0xF5,0xF6,0xF7,0xF8,0xF9,0xFA,0xFB,0xFC,0xFD,0xFE,0xFF} #elif _CODE_PAGE == 858 /* Multilingual Latin 1 + Euro (OEM) */ #define _DF1S 0 #define _EXCVT {0x80,0x9A,0x90,0xB6,0x8E,0xB7,0x8F,0x80,0xD2,0xD3,0xD4,0xD8,0xD7,0xDE,0x8E,0x8F,0x90,0x92,0x92,0xE2,0x99,0xE3,0xEA,0xEB,0x59,0x99,0x9A,0x9D,0x9C,0x9D,0x9E,0x9F, \ 0xB5,0xD6,0xE0,0xE9,0xA5,0xA5,0xA6,0xA7,0xA8,0xA9,0xAA,0xAB,0xAC,0x21,0xAE,0xAF,0xB0,0xB1,0xB2,0xB3,0xB4,0xB5,0xB6,0xB7,0xB8,0xB9,0xBA,0xBB,0xBC,0xBD,0xBE,0xBF, \ 0xC0,0xC1,0xC2,0xC3,0xC4,0xC5,0xC7,0xC7,0xC8,0xC9,0xCA,0xCB,0xCC,0xCD,0xCE,0xCF,0xD1,0xD1,0xD2,0xD3,0xD4,0xD5,0xD6,0xD7,0xD8,0xD9,0xDA,0xDB,0xDC,0xDD,0xDE,0xDF, \ 0xE0,0xE1,0xE2,0xE3,0xE5,0xE5,0xE6,0xE7,0xE7,0xE9,0xEA,0xEB,0xED,0xED,0xEE,0xEF,0xF0,0xF1,0xF2,0xF3,0xF4,0xF5,0xF6,0xF7,0xF8,0xF9,0xFA,0xFB,0xFC,0xFD,0xFE,0xFF} #elif _CODE_PAGE == 862 /* Hebrew (OEM) */ #define _DF1S 0 #define _EXCVT {0x80,0x81,0x82,0x83,0x84,0x85,0x86,0x87,0x88,0x89,0x8A,0x8B,0x8C,0x8D,0x8E,0x8F,0x90,0x91,0x92,0x93,0x94,0x95,0x96,0x97,0x98,0x99,0x9A,0x9B,0x9C,0x9D,0x9E,0x9F, \ 0x41,0x49,0x4F,0x55,0xA5,0xA5,0xA6,0xA7,0xA8,0xA9,0xAA,0xAB,0xAC,0x21,0xAE,0xAF,0xB0,0xB1,0xB2,0xB3,0xB4,0xB5,0xB6,0xB7,0xB8,0xB9,0xBA,0xBB,0xBC,0xBD,0xBE,0xBF, \ 0xC0,0xC1,0xC2,0xC3,0xC4,0xC5,0xC6,0xC7,0xC8,0xC9,0xCA,0xCB,0xCC,0xCD,0xCE,0xCF,0xD0,0xD1,0xD2,0xD3,0xD4,0xD5,0xD6,0xD7,0xD8,0xD9,0xDA,0xDB,0xDC,0xDD,0xDE,0xDF, \ 0xE0,0xE1,0xE2,0xE3,0xE4,0xE5,0xE6,0xE7,0xE8,0xE9,0xEA,0xEB,0xEC,0xED,0xEE,0xEF,0xF0,0xF1,0xF2,0xF3,0xF4,0xF5,0xF6,0xF7,0xF8,0xF9,0xFA,0xFB,0xFC,0xFD,0xFE,0xFF} #elif _CODE_PAGE == 866 /* Russian (OEM) */ #define _DF1S 0 #define _EXCVT {0x80,0x81,0x82,0x83,0x84,0x85,0x86,0x87,0x88,0x89,0x8A,0x8B,0x8C,0x8D,0x8E,0x8F,0x90,0x91,0x92,0x93,0x94,0x95,0x96,0x97,0x98,0x99,0x9A,0x9B,0x9C,0x9D,0x9E,0x9F, \ 0x80,0x81,0x82,0x83,0x84,0x85,0x86,0x87,0x88,0x89,0x8A,0x8B,0x8C,0x8D,0x8E,0x8F,0xB0,0xB1,0xB2,0xB3,0xB4,0xB5,0xB6,0xB7,0xB8,0xB9,0xBA,0xBB,0xBC,0xBD,0xBE,0xBF, \ 0xC0,0xC1,0xC2,0xC3,0xC4,0xC5,0xC6,0xC7,0xC8,0xC9,0xCA,0xCB,0xCC,0xCD,0xCE,0xCF,0xD0,0xD1,0xD2,0xD3,0xD4,0xD5,0xD6,0xD7,0xD8,0xD9,0xDA,0xDB,0xDC,0xDD,0xDE,0xDF, \ 0x90,0x91,0x92,0x93,0x9d,0x95,0x96,0x97,0x98,0x99,0x9A,0x9B,0x9C,0x9D,0x9E,0x9F,0xF0,0xF0,0xF2,0xF2,0xF4,0xF4,0xF6,0xF6,0xF8,0xF9,0xFA,0xFB,0xFC,0xFD,0xFE,0xFF} #elif _CODE_PAGE == 874 /* Thai (OEM, Windows) */ #define _DF1S 0 #define _EXCVT {0x80,0x81,0x82,0x83,0x84,0x85,0x86,0x87,0x88,0x89,0x8A,0x8B,0x8C,0x8D,0x8E,0x8F,0x90,0x91,0x92,0x93,0x94,0x95,0x96,0x97,0x98,0x99,0x9A,0x9B,0x9C,0x9D,0x9E,0x9F, \ 0xA0,0xA1,0xA2,0xA3,0xA4,0xA5,0xA6,0xA7,0xA8,0xA9,0xAA,0xAB,0xAC,0xAD,0xAE,0xAF,0xB0,0xB1,0xB2,0xB3,0xB4,0xB5,0xB6,0xB7,0xB8,0xB9,0xBA,0xBB,0xBC,0xBD,0xBE,0xBF, \ 0xC0,0xC1,0xC2,0xC3,0xC4,0xC5,0xC6,0xC7,0xC8,0xC9,0xCA,0xCB,0xCC,0xCD,0xCE,0xCF,0xD0,0xD1,0xD2,0xD3,0xD4,0xD5,0xD6,0xD7,0xD8,0xD9,0xDA,0xDB,0xDC,0xDD,0xDE,0xDF, \ 0xE0,0xE1,0xE2,0xE3,0xE4,0xE5,0xE6,0xE7,0xE8,0xE9,0xEA,0xEB,0xEC,0xED,0xEE,0xEF,0xF0,0xF1,0xF2,0xF3,0xF4,0xF5,0xF6,0xF7,0xF8,0xF9,0xFA,0xFB,0xFC,0xFD,0xFE,0xFF} #elif _CODE_PAGE == 1250 /* Central Europe (Windows) */ #define _DF1S 0 #define _EXCVT {0x80,0x81,0x82,0x83,0x84,0x85,0x86,0x87,0x88,0x89,0x8A,0x8B,0x8C,0x8D,0x8E,0x8F,0x90,0x91,0x92,0x93,0x94,0x95,0x96,0x97,0x98,0x99,0x8A,0x9B,0x8C,0x8D,0x8E,0x8F, \ 0xA0,0xA1,0xA2,0xA3,0xA4,0xA5,0xA6,0xA7,0xA8,0xA9,0xAA,0xAB,0xAC,0xAD,0xAE,0xAF,0xB0,0xB1,0xB2,0xA3,0xB4,0xB5,0xB6,0xB7,0xB8,0xA5,0xAA,0xBB,0xBC,0xBD,0xBC,0xAF, \ 0xC0,0xC1,0xC2,0xC3,0xC4,0xC5,0xC6,0xC7,0xC8,0xC9,0xCA,0xCB,0xCC,0xCD,0xCE,0xCF,0xD0,0xD1,0xD2,0xD3,0xD4,0xD5,0xD6,0xD7,0xD8,0xD9,0xDA,0xDB,0xDC,0xDD,0xDE,0xDF, \ 0xC0,0xC1,0xC2,0xC3,0xC4,0xC5,0xC6,0xC7,0xC8,0xC9,0xCA,0xCB,0xCC,0xCD,0xCE,0xCF,0xD0,0xD1,0xD2,0xD3,0xD4,0xD5,0xD6,0xF7,0xD8,0xD9,0xDA,0xDB,0xDC,0xDD,0xDE,0xFF} #elif _CODE_PAGE == 1251 /* Cyrillic (Windows) */ #define _DF1S 0 #define _EXCVT {0x80,0x81,0x82,0x82,0x84,0x85,0x86,0x87,0x88,0x89,0x8A,0x8B,0x8C,0x8D,0x8E,0x8F,0x80,0x91,0x92,0x93,0x94,0x95,0x96,0x97,0x98,0x99,0x8A,0x9B,0x8C,0x8D,0x8E,0x8F, \ 0xA0,0xA2,0xA2,0xA3,0xA4,0xA5,0xA6,0xA7,0xA8,0xA9,0xAA,0xAB,0xAC,0xAD,0xAE,0xAF,0xB0,0xB1,0xB2,0xB2,0xA5,0xB5,0xB6,0xB7,0xA8,0xB9,0xAA,0xBB,0xA3,0xBD,0xBD,0xAF, \ 0xC0,0xC1,0xC2,0xC3,0xC4,0xC5,0xC6,0xC7,0xC8,0xC9,0xCA,0xCB,0xCC,0xCD,0xCE,0xCF,0xD0,0xD1,0xD2,0xD3,0xD4,0xD5,0xD6,0xD7,0xD8,0xD9,0xDA,0xDB,0xDC,0xDD,0xDE,0xDF, \ 0xC0,0xC1,0xC2,0xC3,0xC4,0xC5,0xC6,0xC7,0xC8,0xC9,0xCA,0xCB,0xCC,0xCD,0xCE,0xCF,0xD0,0xD1,0xD2,0xD3,0xD4,0xD5,0xD6,0xD7,0xD8,0xD9,0xDA,0xDB,0xDC,0xDD,0xDE,0xDF} #elif _CODE_PAGE == 1252 /* Latin 1 (Windows) */ #define _DF1S 0 #define _EXCVT {0x80,0x81,0x82,0x83,0x84,0x85,0x86,0x87,0x88,0x89,0x8A,0x8B,0x8C,0x8D,0x8E,0x8F,0x90,0x91,0x92,0x93,0x94,0x95,0x96,0x97,0x98,0x99,0xAd,0x9B,0x8C,0x9D,0xAE,0x9F, \ 0xA0,0x21,0xA2,0xA3,0xA4,0xA5,0xA6,0xA7,0xA8,0xA9,0xAA,0xAB,0xAC,0xAD,0xAE,0xAF,0xB0,0xB1,0xB2,0xB3,0xB4,0xB5,0xB6,0xB7,0xB8,0xB9,0xBA,0xBB,0xBC,0xBD,0xBE,0xBF, \ 0xC0,0xC1,0xC2,0xC3,0xC4,0xC5,0xC6,0xC7,0xC8,0xC9,0xCA,0xCB,0xCC,0xCD,0xCE,0xCF,0xD0,0xD1,0xD2,0xD3,0xD4,0xD5,0xD6,0xD7,0xD8,0xD9,0xDA,0xDB,0xDC,0xDD,0xDE,0xDF, \ 0xC0,0xC1,0xC2,0xC3,0xC4,0xC5,0xC6,0xC7,0xC8,0xC9,0xCA,0xCB,0xCC,0xCD,0xCE,0xCF,0xD0,0xD1,0xD2,0xD3,0xD4,0xD5,0xD6,0xF7,0xD8,0xD9,0xDA,0xDB,0xDC,0xDD,0xDE,0x9F} #elif _CODE_PAGE == 1253 /* Greek (Windows) */ #define _DF1S 0 #define _EXCVT {0x80,0x81,0x82,0x83,0x84,0x85,0x86,0x87,0x88,0x89,0x8A,0x8B,0x8C,0x8D,0x8E,0x8F,0x90,0x91,0x92,0x93,0x94,0x95,0x96,0x97,0x98,0x99,0x9A,0x9B,0x9C,0x9D,0x9E,0x9F, \ 0xA0,0xA1,0xA2,0xA3,0xA4,0xA5,0xA6,0xA7,0xA8,0xA9,0xAA,0xAB,0xAC,0xAD,0xAE,0xAF,0xB0,0xB1,0xB2,0xB3,0xB4,0xB5,0xB6,0xB7,0xB8,0xB9,0xBA,0xBB,0xBC,0xBD,0xBE,0xBF, \ 0xC0,0xC1,0xC2,0xC3,0xC4,0xC5,0xC6,0xC7,0xC8,0xC9,0xCA,0xCB,0xCC,0xCD,0xCE,0xCF,0xD0,0xD1,0xD2,0xD3,0xD4,0xD5,0xD6,0xD7,0xD8,0xD9,0xDA,0xDB,0xA2,0xB8,0xB9,0xBA, \ 0xE0,0xC1,0xC2,0xC3,0xC4,0xC5,0xC6,0xC7,0xC8,0xC9,0xCA,0xCB,0xCC,0xCD,0xCE,0xCF,0xD0,0xD1,0xF2,0xD3,0xD4,0xD5,0xD6,0xD7,0xD8,0xD9,0xDA,0xFB,0xBC,0xFD,0xBF,0xFF} #elif _CODE_PAGE == 1254 /* Turkish (Windows) */ #define _DF1S 0 #define _EXCVT {0x80,0x81,0x82,0x83,0x84,0x85,0x86,0x87,0x88,0x89,0x8A,0x8B,0x8C,0x8D,0x8E,0x8F,0x90,0x91,0x92,0x93,0x94,0x95,0x96,0x97,0x98,0x99,0x8A,0x9B,0x8C,0x9D,0x9E,0x9F, \ 0xA0,0x21,0xA2,0xA3,0xA4,0xA5,0xA6,0xA7,0xA8,0xA9,0xAA,0xAB,0xAC,0xAD,0xAE,0xAF,0xB0,0xB1,0xB2,0xB3,0xB4,0xB5,0xB6,0xB7,0xB8,0xB9,0xBA,0xBB,0xBC,0xBD,0xBE,0xBF, \ 0xC0,0xC1,0xC2,0xC3,0xC4,0xC5,0xC6,0xC7,0xC8,0xC9,0xCA,0xCB,0xCC,0xCD,0xCE,0xCF,0xD0,0xD1,0xD2,0xD3,0xD4,0xD5,0xD6,0xD7,0xD8,0xD9,0xDA,0xDB,0xDC,0xDD,0xDE,0xDF, \ 0xC0,0xC1,0xC2,0xC3,0xC4,0xC5,0xC6,0xC7,0xC8,0xC9,0xCA,0xCB,0xCC,0xCD,0xCE,0xCF,0xD0,0xD1,0xD2,0xD3,0xD4,0xD5,0xD6,0xF7,0xD8,0xD9,0xDA,0xDB,0xDC,0xDD,0xDE,0x9F} #elif _CODE_PAGE == 1255 /* Hebrew (Windows) */ #define _DF1S 0 #define _EXCVT {0x80,0x81,0x82,0x83,0x84,0x85,0x86,0x87,0x88,0x89,0x8A,0x8B,0x8C,0x8D,0x8E,0x8F,0x90,0x91,0x92,0x93,0x94,0x95,0x96,0x97,0x98,0x99,0x9A,0x9B,0x9C,0x9D,0x9E,0x9F, \ 0xA0,0x21,0xA2,0xA3,0xA4,0xA5,0xA6,0xA7,0xA8,0xA9,0xAA,0xAB,0xAC,0xAD,0xAE,0xAF,0xB0,0xB1,0xB2,0xB3,0xB4,0xB5,0xB6,0xB7,0xB8,0xB9,0xBA,0xBB,0xBC,0xBD,0xBE,0xBF, \ 0xC0,0xC1,0xC2,0xC3,0xC4,0xC5,0xC6,0xC7,0xC8,0xC9,0xCA,0xCB,0xCC,0xCD,0xCE,0xCF,0xD0,0xD1,0xD2,0xD3,0xD4,0xD5,0xD6,0xD7,0xD8,0xD9,0xDA,0xDB,0xDC,0xDD,0xDE,0xDF, \ 0xE0,0xE1,0xE2,0xE3,0xE4,0xE5,0xE6,0xE7,0xE8,0xE9,0xEA,0xEB,0xEC,0xED,0xEE,0xEF,0xF0,0xF1,0xF2,0xF3,0xF4,0xF5,0xF6,0xF7,0xF8,0xF9,0xFA,0xFB,0xFC,0xFD,0xFE,0xFF} #elif _CODE_PAGE == 1256 /* Arabic (Windows) */ #define _DF1S 0 #define _EXCVT {0x80,0x81,0x82,0x83,0x84,0x85,0x86,0x87,0x88,0x89,0x8A,0x8B,0x8C,0x8D,0x8E,0x8F,0x90,0x91,0x92,0x93,0x94,0x95,0x96,0x97,0x98,0x99,0x9A,0x9B,0x8C,0x9D,0x9E,0x9F, \ 0xA0,0xA1,0xA2,0xA3,0xA4,0xA5,0xA6,0xA7,0xA8,0xA9,0xAA,0xAB,0xAC,0xAD,0xAE,0xAF,0xB0,0xB1,0xB2,0xB3,0xB4,0xB5,0xB6,0xB7,0xB8,0xB9,0xBA,0xBB,0xBC,0xBD,0xBE,0xBF, \ 0xC0,0xC1,0xC2,0xC3,0xC4,0xC5,0xC6,0xC7,0xC8,0xC9,0xCA,0xCB,0xCC,0xCD,0xCE,0xCF,0xD0,0xD1,0xD2,0xD3,0xD4,0xD5,0xD6,0xD7,0xD8,0xD9,0xDA,0xDB,0xDC,0xDD,0xDE,0xDF, \ 0x41,0xE1,0x41,0xE3,0xE4,0xE5,0xE6,0x43,0x45,0x45,0x45,0x45,0xEC,0xED,0x49,0x49,0xF0,0xF1,0xF2,0xF3,0x4F,0xF5,0xF6,0xF7,0xF8,0x55,0xFA,0x55,0x55,0xFD,0xFE,0xFF} #elif _CODE_PAGE == 1257 /* Baltic (Windows) */ #define _DF1S 0 #define _EXCVT {0x80,0x81,0x82,0x83,0x84,0x85,0x86,0x87,0x88,0x89,0x8A,0x8B,0x8C,0x8D,0x8E,0x8F,0x90,0x91,0x92,0x93,0x94,0x95,0x96,0x97,0x98,0x99,0x9A,0x9B,0x9C,0x9D,0x9E,0x9F, \ 0xA0,0xA1,0xA2,0xA3,0xA4,0xA5,0xA6,0xA7,0xA8,0xA9,0xAA,0xAB,0xAC,0xAD,0xAE,0xAF,0xB0,0xB1,0xB2,0xB3,0xB4,0xB5,0xB6,0xB7,0xA8,0xB9,0xAA,0xBB,0xBC,0xBD,0xBE,0xAF, \ 0xC0,0xC1,0xC2,0xC3,0xC4,0xC5,0xC6,0xC7,0xC8,0xC9,0xCA,0xCB,0xCC,0xCD,0xCE,0xCF,0xD0,0xD1,0xD2,0xD3,0xD4,0xD5,0xD6,0xD7,0xD8,0xD9,0xDA,0xDB,0xDC,0xDD,0xDE,0xDF, \ 0xC0,0xC1,0xC2,0xC3,0xC4,0xC5,0xC6,0xC7,0xC8,0xC9,0xCA,0xCB,0xCC,0xCD,0xCE,0xCF,0xD0,0xD1,0xD2,0xD3,0xD4,0xD5,0xD6,0xF7,0xD8,0xD9,0xDA,0xDB,0xDC,0xDD,0xDE,0xFF} #elif _CODE_PAGE == 1258 /* Vietnam (OEM, Windows) */ #define _DF1S 0 #define _EXCVT {0x80,0x81,0x82,0x83,0x84,0x85,0x86,0x87,0x88,0x89,0x8A,0x8B,0x8C,0x8D,0x8E,0x8F,0x90,0x91,0x92,0x93,0x94,0x95,0x96,0x97,0x98,0x99,0x9A,0x9B,0xAC,0x9D,0x9E,0x9F, \ 0xA0,0x21,0xA2,0xA3,0xA4,0xA5,0xA6,0xA7,0xA8,0xA9,0xAA,0xAB,0xAC,0xAD,0xAE,0xAF,0xB0,0xB1,0xB2,0xB3,0xB4,0xB5,0xB6,0xB7,0xB8,0xB9,0xBA,0xBB,0xBC,0xBD,0xBE,0xBF, \ 0xC0,0xC1,0xC2,0xC3,0xC4,0xC5,0xC6,0xC7,0xC8,0xC9,0xCA,0xCB,0xCC,0xCD,0xCE,0xCF,0xD0,0xD1,0xD2,0xD3,0xD4,0xD5,0xD6,0xD7,0xD8,0xD9,0xDA,0xDB,0xDC,0xDD,0xDE,0xDF, \ 0xC0,0xC1,0xC2,0xC3,0xC4,0xC5,0xC6,0xC7,0xC8,0xC9,0xCA,0xCB,0xEC,0xCD,0xCE,0xCF,0xD0,0xD1,0xF2,0xD3,0xD4,0xD5,0xD6,0xF7,0xD8,0xD9,0xDA,0xDB,0xDC,0xDD,0xFE,0x9F} #elif _CODE_PAGE == 1 /* ASCII (for only non-LFN cfg) */ #define _DF1S 0 #else #error Unknown code page #endif /* Character code support macros */ #define IsUpper(c) (((c)>='A')&&((c)<='Z')) #define IsLower(c) (((c)>='a')&&((c)<='z')) #if _DF1S /* DBCS configuration */ #ifdef _DF2S /* Two 1st byte areas */ #define IsDBCS1(c) (((BYTE)(c) >= _DF1S && (BYTE)(c) <= _DF1E) || ((BYTE)(c) >= _DF2S && (BYTE)(c) <= _DF2E)) #else /* One 1st byte area */ #define IsDBCS1(c) ((BYTE)(c) >= _DF1S && (BYTE)(c) <= _DF1E) #endif #ifdef _DS3S /* Three 2nd byte areas */ #define IsDBCS2(c) (((BYTE)(c) >= _DS1S && (BYTE)(c) <= _DS1E) || ((BYTE)(c) >= _DS2S && (BYTE)(c) <= _DS2E) || ((BYTE)(c) >= _DS3S && (BYTE)(c) <= _DS3E)) #else /* Two 2nd byte areas */ #define IsDBCS2(c) (((BYTE)(c) >= _DS1S && (BYTE)(c) <= _DS1E) || ((BYTE)(c) >= _DS2S && (BYTE)(c) <= _DS2E)) #endif #else /* SBCS configuration */ #define IsDBCS1(c) 0 #define IsDBCS2(c) 0 #endif /* _DF1S */ /* FatFs refers the members in the FAT structures with byte offset instead / of structure member because there are incompatibility of the packing option / between various compilers. */ #define BS_jmpBoot 0 #define BS_OEMName 3 #define BPB_BytsPerSec 11 #define BPB_SecPerClus 13 #define BPB_RsvdSecCnt 14 #define BPB_NumFATs 16 #define BPB_RootEntCnt 17 #define BPB_TotSec16 19 #define BPB_Media 21 #define BPB_FATSz16 22 #define BPB_SecPerTrk 24 #define BPB_NumHeads 26 #define BPB_HiddSec 28 #define BPB_TotSec32 32 #define BS_55AA 510 #define BS_DrvNum 36 #define BS_BootSig 38 #define BS_VolID 39 #define BS_VolLab 43 #define BS_FilSysType 54 #define BPB_FATSz32 36 #define BPB_ExtFlags 40 #define BPB_FSVer 42 #define BPB_RootClus 44 #define BPB_FSInfo 48 #define BPB_BkBootSec 50 #define BS_DrvNum32 64 #define BS_BootSig32 66 #define BS_VolID32 67 #define BS_VolLab32 71 #define BS_FilSysType32 82 #define MBR_Table 446 #define DIR_Name 0 #define DIR_Attr 11 #define DIR_NTres 12 #define DIR_CrtTime 14 #define DIR_CrtDate 16 #define DIR_FstClusHI 20 #define DIR_WrtTime 22 #define DIR_WrtDate 24 #define DIR_FstClusLO 26 #define DIR_FileSize 28 /*-------------------------------------------------------------------------- Private Functions ---------------------------------------------------------------------------*/ static FATFS *FatFs; /* Pointer to the file system object (logical drive) */ /* Fill memory */ static void mem_set (void* dst, int val, int cnt) { char *d = (char*)dst; while (cnt--) *d++ = (char)val; } /* Compare memory to memory */ static int mem_cmp (const void* dst, const void* src, int cnt) { const char *d = (const char *)dst, *s = (const char *)src; int r = 0; while (cnt-- && (r = *d++ - *s++) == 0) ; return r; } /*-----------------------------------------------------------------------*/ /* FAT access - Read value of a FAT entry */ /*-----------------------------------------------------------------------*/ static CLUST get_fat ( /* 1:IO error, Else:Cluster status */ CLUST clst /* Cluster# to get the link information */ ) { #if _FS_FAT12 WORD wc, bc, ofs; #endif BYTE buf[4]; FATFS *fs = FatFs; if (clst < 2 || clst >= fs->n_fatent) /* Range check */ return 1; switch (fs->fs_type) { #if _FS_FAT12 case FS_FAT12 : bc = (WORD)clst; bc += bc / 2; ofs = bc % 512; bc /= 512; if (ofs != 511) { if (disk_readp(buf, fs->fatbase + bc, ofs, 2)) break; } else { if (disk_readp(buf, fs->fatbase + bc, 511, 1)) break; if (disk_readp(buf+1, fs->fatbase + bc + 1, 0, 1)) break; } wc = LD_WORD(buf); return (clst & 1) ? (wc >> 4) : (wc & 0xFFF); #endif case FS_FAT16 : if (disk_readp(buf, fs->fatbase + clst / 256, (WORD)(((WORD)clst % 256) * 2), 2)) break; return LD_WORD(buf); #if _FS_FAT32 case FS_FAT32 : if (disk_readp(buf, fs->fatbase + clst / 128, (WORD)(((WORD)clst % 128) * 4), 4)) break; return LD_DWORD(buf) & 0x0FFFFFFF; #endif } return 1; /* An error occured at the disk I/O layer */ } /*-----------------------------------------------------------------------*/ /* Get sector# from cluster# */ /*-----------------------------------------------------------------------*/ static DWORD clust2sect ( /* !=0: Sector number, 0: Failed - invalid cluster# */ CLUST clst /* Cluster# to be converted */ ) { FATFS *fs = FatFs; clst -= 2; if (clst >= (fs->n_fatent - 2)) return 0; /* Invalid cluster# */ return (DWORD)clst * fs->csize + fs->database; } /*-----------------------------------------------------------------------*/ /* Directory handling - Rewind directory index */ /*-----------------------------------------------------------------------*/ static FRESULT dir_rewind ( DIR *dj /* Pointer to directory object */ ) { CLUST clst; FATFS *fs = FatFs; dj->index = 0; clst = dj->sclust; if (clst == 1 || clst >= fs->n_fatent) /* Check start cluster range */ return FR_DISK_ERR; if (_FS_FAT32 && !clst && fs->fs_type == FS_FAT32) /* Replace cluster# 0 with root cluster# if in FAT32 */ clst = (CLUST)fs->dirbase; dj->clust = clst; /* Current cluster */ dj->sect = clst ? clust2sect(clst) : fs->dirbase; /* Current sector */ return FR_OK; /* Seek succeeded */ } /*-----------------------------------------------------------------------*/ /* Directory handling - Move directory index next */ /*-----------------------------------------------------------------------*/ static FRESULT dir_next ( /* FR_OK:Succeeded, FR_NO_FILE:End of table */ DIR *dj /* Pointer to directory object */ ) { CLUST clst; WORD i; FATFS *fs = FatFs; i = dj->index + 1; if (!i || !dj->sect) /* Report EOT when index has reached 65535 */ return FR_NO_FILE; if (!(i % 16)) { /* Sector changed? */ dj->sect++; /* Next sector */ if (dj->clust == 0) { /* Static table */ if (i >= fs->n_rootdir) /* Report EOT when end of table */ return FR_NO_FILE; } else { /* Dynamic table */ if (((i / 16) & (fs->csize-1)) == 0) { /* Cluster changed? */ clst = get_fat(dj->clust); /* Get next cluster */ if (clst <= 1) return FR_DISK_ERR; if (clst >= fs->n_fatent) /* When it reached end of dynamic table */ return FR_NO_FILE; /* Report EOT */ dj->clust = clst; /* Initialize data for new cluster */ dj->sect = clust2sect(clst); } } } dj->index = i; return FR_OK; } /*-----------------------------------------------------------------------*/ /* Directory handling - Find an object in the directory */ /*-----------------------------------------------------------------------*/ static FRESULT dir_find ( DIR *dj, /* Pointer to the directory object linked to the file name */ BYTE *dir /* 32-byte working buffer */ ) { FRESULT res; BYTE c; res = dir_rewind(dj); /* Rewind directory object */ if (res != FR_OK) return res; do { res = disk_readp(dir, dj->sect, (WORD)((dj->index % 16) * 32), 32) /* Read an entry */ ? FR_DISK_ERR : FR_OK; if (res != FR_OK) break; c = dir[DIR_Name]; /* First character */ if (c == 0) { res = FR_NO_FILE; break; } /* Reached to end of table */ if (!(dir[DIR_Attr] & AM_VOL) && !mem_cmp(dir, dj->fn, 11)) /* Is it a valid entry? */ break; res = dir_next(dj); /* Next entry */ } while (res == FR_OK); return res; } /*-----------------------------------------------------------------------*/ /* Read an object from the directory */ /*-----------------------------------------------------------------------*/ #if _USE_DIR static FRESULT dir_read ( DIR *dj, /* Pointer to the directory object to store read object name */ BYTE *dir /* 32-byte working buffer */ ) { FRESULT res; BYTE a, c; res = FR_NO_FILE; while (dj->sect) { res = disk_readp(dir, dj->sect, (WORD)((dj->index % 16) * 32), 32) /* Read an entry */ ? FR_DISK_ERR : FR_OK; if (res != FR_OK) break; c = dir[DIR_Name]; if (c == 0) { res = FR_NO_FILE; break; } /* Reached to end of table */ a = dir[DIR_Attr] & AM_MASK; if (c != 0xE5 && c != '.' && !(a & AM_VOL)) /* Is it a valid entry? */ break; res = dir_next(dj); /* Next entry */ if (res != FR_OK) break; } if (res != FR_OK) dj->sect = 0; return res; } #endif /*-----------------------------------------------------------------------*/ /* Pick a segment and create the object name in directory form */ /*-----------------------------------------------------------------------*/ #ifdef _EXCVT static const BYTE cvt[] = _EXCVT; #endif static FRESULT create_name ( DIR *dj, /* Pointer to the directory object */ const char **path /* Pointer to pointer to the segment in the path string */ ) { BYTE c, d, ni, si, i, *sfn; const char *p; /* Create file name in directory form */ sfn = dj->fn; mem_set(sfn, ' ', 11); si = i = 0; ni = 8; p = *path; for (;;) { c = p[si++]; if (c <= ' ' || c == '/') break; /* Break on end of segment */ if (c == '.' || i >= ni) { if (ni != 8 || c != '.') break; i = 8; ni = 11; continue; } #ifdef _EXCVT if (c >= 0x80) /* To upper extended char (SBCS) */ c = cvt[c - 0x80]; #endif if (IsDBCS1(c) && i < ni - 1) { /* DBC 1st byte? */ d = p[si++]; /* Get 2nd byte */ sfn[i++] = c; sfn[i++] = d; } else { /* Single byte code */ if (IsLower(c)) c -= 0x20; /* toupper */ sfn[i++] = c; } } *path = &p[si]; /* Rerurn pointer to the next segment */ sfn[11] = (c <= ' ') ? 1 : 0; /* Set last segment flag if end of path */ return FR_OK; } /*-----------------------------------------------------------------------*/ /* Get file information from directory entry */ /*-----------------------------------------------------------------------*/ #if _USE_DIR static void get_fileinfo ( /* No return code */ DIR *dj, /* Pointer to the directory object */ BYTE *dir, /* 32-byte working buffer */ FILINFO *fno /* Pointer to store the file information */ ) { BYTE i, c; char *p; p = fno->fname; if (dj->sect) { for (i = 0; i < 8; i++) { /* Copy file name body */ c = dir[i]; if (c == ' ') break; if (c == 0x05) c = 0xE5; *p++ = c; } if (dir[8] != ' ') { /* Copy file name extension */ *p++ = '.'; for (i = 8; i < 11; i++) { c = dir[i]; if (c == ' ') break; *p++ = c; } } fno->fattrib = dir[DIR_Attr]; /* Attribute */ fno->fsize = LD_DWORD(dir+DIR_FileSize); /* Size */ fno->fdate = LD_WORD(dir+DIR_WrtDate); /* Date */ fno->ftime = LD_WORD(dir+DIR_WrtTime); /* Time */ } *p = 0; } #endif /* _USE_DIR */ /*-----------------------------------------------------------------------*/ /* Follow a file path */ /*-----------------------------------------------------------------------*/ static FRESULT follow_path ( /* FR_OK(0): successful, !=0: error code */ DIR *dj, /* Directory object to return last directory and found object */ BYTE *dir, /* 32-byte working buffer */ const char *path /* Full-path string to find a file or directory */ ) { FRESULT res; while (*path == ' ') path++; /* Skip leading spaces */ if (*path == '/') path++; /* Strip heading separator */ dj->sclust = 0; /* Set start directory (always root dir) */ if ((BYTE)*path <= ' ') { /* Null path means the root directory */ res = dir_rewind(dj); dir[0] = 0; } else { /* Follow path */ for (;;) { res = create_name(dj, &path); /* Get a segment */ if (res != FR_OK) break; res = dir_find(dj, dir); /* Find it */ if (res != FR_OK) { /* Could not find the object */ if (res == FR_NO_FILE && !*(dj->fn+11)) res = FR_NO_PATH; break; } if (*(dj->fn+11)) break; /* Last segment match. Function completed. */ if (!(dir[DIR_Attr] & AM_DIR)) { /* Cannot follow because it is a file */ res = FR_NO_PATH; break; } dj->sclust = LD_CLUST(dir); } } return res; } /*-----------------------------------------------------------------------*/ /* Check a sector if it is an FAT boot record */ /*-----------------------------------------------------------------------*/ static BYTE check_fs ( /* 0:The FAT boot record, 1:Valid boot record but not an FAT, 2:Not a boot record, 3:Error */ BYTE *buf, /* Working buffer */ DWORD sect /* Sector# (lba) to check if it is an FAT boot record or not */ ) { if (disk_readp(buf, sect, 510, 2)) /* Read the boot sector */ return 3; if (LD_WORD(buf) != 0xAA55) /* Check record signature */ return 2; if (!disk_readp(buf, sect, BS_FilSysType, 2) && LD_WORD(buf) == 0x4146) /* Check FAT12/16 */ return 0; if (_FS_FAT32 && !disk_readp(buf, sect, BS_FilSysType32, 2) && LD_WORD(buf) == 0x4146) /* Check FAT32 */ return 0; return 1; } /*-------------------------------------------------------------------------- Public Functions --------------------------------------------------------------------------*/ /*-----------------------------------------------------------------------*/ /* Mount/Unmount a Locical Drive */ /*-----------------------------------------------------------------------*/ FRESULT pf_mount ( FATFS *fs /* Pointer to new file system object (NULL: Unmount) */ ) { BYTE fmt, buf[36]; DWORD bsect, fsize, tsect, mclst; BYTE resTest; FatFs = 0; if (!fs) return FR_OK; /* Unregister fs object */ resTest = disk_initialize() ; if (resTest& STA_NOINIT) /* Check if the drive is ready or not */ return FR_NOT_READY; /* Search FAT partition on the drive */ bsect = 0; fmt = check_fs(buf, bsect); /* Check sector 0 as an SFD format */ if (fmt == 1) { /* Not an FAT boot record, it may be FDISK format */ /* Check a partition listed in top of the partition table */ if (disk_readp(buf, bsect, MBR_Table, 16)) { /* 1st partition entry */ fmt = 3; } else { if (buf[4]) { /* Is the partition existing? */ bsect = LD_DWORD(&buf[8]); /* Partition offset in LBA */ fmt = check_fs(buf, bsect); /* Check the partition */ } } } if (fmt == 3) return FR_DISK_ERR; if (fmt) return FR_NO_FILESYSTEM; /* No valid FAT patition is found */ /* Initialize the file system object */ if (disk_readp(buf, bsect, 13, sizeof(buf))) return FR_DISK_ERR; fsize = LD_WORD(buf+BPB_FATSz16-13); /* Number of sectors per FAT */ if (!fsize) fsize = LD_DWORD(buf+BPB_FATSz32-13); fsize *= buf[BPB_NumFATs-13]; /* Number of sectors in FAT area */ fs->fatbase = bsect + LD_WORD(buf+BPB_RsvdSecCnt-13); /* FAT start sector (lba) */ fs->csize = buf[BPB_SecPerClus-13]; /* Number of sectors per cluster */ fs->n_rootdir = LD_WORD(buf+BPB_RootEntCnt-13); /* Nmuber of root directory entries */ tsect = LD_WORD(buf+BPB_TotSec16-13); /* Number of sectors on the file system */ if (!tsect) tsect = LD_DWORD(buf+BPB_TotSec32-13); mclst = (tsect /* Last cluster# + 1 */ - LD_WORD(buf+BPB_RsvdSecCnt-13) - fsize - fs->n_rootdir / 16 ) / fs->csize + 2; fs->n_fatent = (CLUST)mclst; fmt = FS_FAT16; /* Determine the FAT sub type */ if (mclst < 0xFF7) /* Number of clusters < 0xFF5 */ #if _FS_FAT12 fmt = FS_FAT12; #else return FR_NO_FILESYSTEM; #endif if (mclst >= 0xFFF7) /* Number of clusters >= 0xFFF5 */ #if _FS_FAT32 fmt = FS_FAT32; #else return FR_NO_FILESYSTEM; #endif fs->fs_type = fmt; /* FAT sub-type */ if (_FS_FAT32 && fmt == FS_FAT32) fs->dirbase = LD_DWORD(buf+(BPB_RootClus-13)); /* Root directory start cluster */ else fs->dirbase = fs->fatbase + fsize; /* Root directory start sector (lba) */ fs->database = fs->fatbase + fsize + fs->n_rootdir / 16; /* Data start sector (lba) */ fs->flag = 0; FatFs = fs; return FR_OK; } /*-----------------------------------------------------------------------*/ /* Open or Create a File */ /*-----------------------------------------------------------------------*/ FRESULT pf_open ( const char *path /* Pointer to the file name */ ) { FRESULT res; DIR dj; BYTE sp[12], dir[32]; FATFS *fs = FatFs; if (!fs) /* Check file system */ return FR_NOT_ENABLED; fs->flag = 0; dj.fn = sp; res = follow_path(&dj, dir, path); /* Follow the file path */ if (res != FR_OK) return res; /* Follow failed */ if (!dir[0] || (dir[DIR_Attr] & AM_DIR)) /* It is a directory */ return FR_NO_FILE; fs->org_clust = LD_CLUST(dir); /* File start cluster */ fs->fsize = LD_DWORD(dir+DIR_FileSize); /* File size */ fs->fptr = 0; /* File pointer */ fs->flag = FA_OPENED; return FR_OK; } /*-----------------------------------------------------------------------*/ /* Read File */ /*-----------------------------------------------------------------------*/ #if _USE_READ FRESULT pf_read ( void* buff, /* Pointer to the read buffer (NULL:Forward data to the stream)*/ WORD btr, /* Number of bytes to read */ WORD* br /* Pointer to number of bytes read */ ) { DRESULT dr; CLUST clst; DWORD sect, remain; WORD rcnt; BYTE cs, *rbuff = buff; FATFS *fs = FatFs; *br = 0; if (!fs) return FR_NOT_ENABLED; /* Check file system */ if (!(fs->flag & FA_OPENED)) /* Check if opened */ return FR_NOT_OPENED; remain = fs->fsize - fs->fptr; if (btr > remain) btr = (WORD)remain; /* Truncate btr by remaining bytes */ while (btr) { /* Repeat until all data transferred */ if ((fs->fptr % 512) == 0) { /* On the sector boundary? */ cs = (BYTE)(fs->fptr / 512 & (fs->csize - 1)); /* Sector offset in the cluster */ if (!cs) { /* On the cluster boundary? */ clst = (fs->fptr == 0) ? /* On the top of the file? */ fs->org_clust : get_fat(fs->curr_clust); if (clst <= 1) goto fr_abort; fs->curr_clust = clst; /* Update current cluster */ } sect = clust2sect(fs->curr_clust); /* Get current sector */ if (!sect) goto fr_abort; fs->dsect = sect + cs; } rcnt = (WORD)(512 - (fs->fptr % 512)); /* Get partial sector data from sector buffer */ if (rcnt > btr) rcnt = btr; dr = disk_readp(!buff ? 0 : rbuff, fs->dsect, (WORD)(fs->fptr % 512), rcnt); if (dr) goto fr_abort; fs->fptr += rcnt; rbuff += rcnt; /* Update pointers and counters */ btr -= rcnt; *br += rcnt; } return FR_OK; fr_abort: fs->flag = 0; return FR_DISK_ERR; } #endif /*-----------------------------------------------------------------------*/ /* Write File */ /*-----------------------------------------------------------------------*/ #if _USE_WRITE FRESULT pf_write ( const void* buff, /* Pointer to the data to be written */ WORD btw, /* Number of bytes to write (0:Finalize the current write operation) */ WORD* bw /* Pointer to number of bytes written */ ) { CLUST clst; DWORD sect, remain; const BYTE *p = buff; BYTE cs; WORD wcnt; FATFS *fs = FatFs; *bw = 0; if (!fs) return FR_NOT_ENABLED; /* Check file system */ if (!(fs->flag & FA_OPENED)) /* Check if opened */ return FR_NOT_OPENED; if (!btw) { /* Finalize request */ if ((fs->flag & FA__WIP) && disk_writep(0, 0)) goto fw_abort; fs->flag &= ~FA__WIP; return FR_OK; } else { /* Write data request */ if (!(fs->flag & FA__WIP)) /* Round-down fptr to the sector boundary */ fs->fptr &= 0xFFFFFE00; } remain = fs->fsize - fs->fptr; if (btw > remain) btw = (WORD)remain; /* Truncate btw by remaining bytes */ while (btw) { /* Repeat until all data transferred */ if (((WORD)fs->fptr % 512) == 0) { /* On the sector boundary? */ cs = (BYTE)(fs->fptr / 512 & (fs->csize - 1)); /* Sector offset in the cluster */ if (!cs) { /* On the cluster boundary? */ clst = (fs->fptr == 0) ? /* On the top of the file? */ fs->org_clust : get_fat(fs->curr_clust); if (clst <= 1) goto fw_abort; fs->curr_clust = clst; /* Update current cluster */ } sect = clust2sect(fs->curr_clust); /* Get current sector */ if (!sect) goto fw_abort; fs->dsect = sect + cs; if (disk_writep(0, fs->dsect)) goto fw_abort; /* Initiate a sector write operation */ fs->flag |= FA__WIP; } wcnt = 512 - ((WORD)fs->fptr % 512); /* Number of bytes to write to the sector */ if (wcnt > btw) wcnt = btw; if (disk_writep(p, wcnt)) goto fw_abort; /* Send data to the sector */ fs->fptr += wcnt; p += wcnt; /* Update pointers and counters */ btw -= wcnt; *bw += wcnt; if (((WORD)fs->fptr % 512) == 0) { if (disk_writep(0, 0)) goto fw_abort; /* Finalize the currtent secter write operation */ fs->flag &= ~FA__WIP; } } return FR_OK; fw_abort: fs->flag = 0; return FR_DISK_ERR; } #endif /*-----------------------------------------------------------------------*/ /* Seek File R/W Pointer */ /*-----------------------------------------------------------------------*/ #if _USE_LSEEK FRESULT pf_lseek ( DWORD ofs /* File pointer from top of file */ ) { CLUST clst; DWORD bcs, sect, ifptr; FATFS *fs = FatFs; if (!fs) return FR_NOT_ENABLED; /* Check file system */ if (!(fs->flag & FA_OPENED)) /* Check if opened */ return FR_NOT_OPENED; if (ofs > fs->fsize) ofs = fs->fsize; /* Clip offset with the file size */ ifptr = fs->fptr; fs->fptr = 0; if (ofs > 0) { bcs = (DWORD)fs->csize * 512; /* Cluster size (byte) */ if (ifptr > 0 && (ofs - 1) / bcs >= (ifptr - 1) / bcs) { /* When seek to same or following cluster, */ fs->fptr = (ifptr - 1) & ~(bcs - 1); /* start from the current cluster */ ofs -= fs->fptr; clst = fs->curr_clust; } else { /* When seek to back cluster, */ clst = fs->org_clust; /* start from the first cluster */ fs->curr_clust = clst; } while (ofs > bcs) { /* Cluster following loop */ clst = get_fat(clst); /* Follow cluster chain */ if (clst <= 1 || clst >= fs->n_fatent) goto fe_abort; fs->curr_clust = clst; fs->fptr += bcs; ofs -= bcs; } fs->fptr += ofs; sect = clust2sect(clst); /* Current sector */ if (!sect) goto fe_abort; fs->dsect = sect + (fs->fptr / 512 & (fs->csize - 1)); } return FR_OK; fe_abort: fs->flag = 0; return FR_DISK_ERR; } #endif /*-----------------------------------------------------------------------*/ /* Create a Directory Object */ /*-----------------------------------------------------------------------*/ #if _USE_DIR FRESULT pf_opendir ( DIR *dj, /* Pointer to directory object to create */ const char *path /* Pointer to the directory path */ ) { FRESULT res; BYTE sp[12], dir[32]; FATFS *fs = FatFs; if (!fs) { /* Check file system */ res = FR_NOT_ENABLED; } else { dj->fn = sp; res = follow_path(dj, dir, path); /* Follow the path to the directory */ if (res == FR_OK) { /* Follow completed */ if (dir[0]) { /* It is not the root dir */ if (dir[DIR_Attr] & AM_DIR) /* The object is a directory */ dj->sclust = LD_CLUST(dir); else /* The object is not a directory */ res = FR_NO_PATH; } if (res == FR_OK) res = dir_rewind(dj); /* Rewind dir */ } if (res == FR_NO_FILE) res = FR_NO_PATH; } return res; } /*-----------------------------------------------------------------------*/ /* Read Directory Entry in Sequense */ /*-----------------------------------------------------------------------*/ FRESULT pf_readdir ( DIR *dj, /* Pointer to the open directory object */ FILINFO *fno /* Pointer to file information to return */ ) { FRESULT res; BYTE sp[12], dir[32]; FATFS *fs = FatFs; if (!fs) { /* Check file system */ res = FR_NOT_ENABLED; } else { dj->fn = sp; if (!fno) { res = dir_rewind(dj); } else { res = dir_read(dj, dir); if (res == FR_NO_FILE) { dj->sect = 0; res = FR_OK; } if (res == FR_OK) { /* A valid entry is found */ get_fileinfo(dj, dir, fno); /* Get the object information */ res = dir_next(dj); /* Increment index for next */ if (res == FR_NO_FILE) { dj->sect = 0; res = FR_OK; } } } } return res; } #endif /* _USE_DIR */
/*****************************************************************/ /********* *********/ /********* FILE: MAIN.C *********/ /********* *********/ /*****************************************************************/ /*****************************************************************/ /********* INCLUDE *********/ /*****************************************************************/ #include <msp430.h> #include <stdint.h> #include "main.h" #include "lcd.h" #include "diskio.h" #include "integer.h" #include "pff.h" #include "spi.h" /*****************************************************************/ /********* MAIN *********/ /*****************************************************************/ int SDCARD_Initialize() { FRESULT res; FATFS fs; // P1DIR |= BIT4; P1SEL |= BIT4; spi_initialize(); // res = disk_initialize(); pf_mount(&fs); res = pf_open("log.txt"); if(res != FR_OK){ LCD_SetText("SDCARD ERROR",1,0); }else{ LCD_SetText("SDCARD OK",1,0); } return 0; } /* * MAIN */ int main(void){ WORD bw; char Line[10]; FRESULT res; WatchDogHold(); LCD_PortConfig(); LCD_Initialize(); LCD_Clear(); SDCARD_Initialize(); res = pf_open("log.txt"); if(res == FR_OK){ LCD_SetText("SDCARD OK",1,0); bw = 0; Line[0] = 66; Line[1] = 65; Line[3] = '\0'; pf_write(Line,strlen(Line),&bw); pf_write(0,0,&bw); } } /*****************************************************************/ /********* GLOBAL FUNCTIONS *********/ /*****************************************************************/ void WatchDogHold(void) { WDTCTL = WDTPW + WDTHOLD; } /*****************************************************************/ /********* END *********/ /*****************************************************************/
/*****************************************************************/ #include "lcd.h" /*****************************************************************/ /********* DEFINES *********/ /*****************************************************************/ #define P1orP2lcd 0x0200 #define EN (PP2 + BIT5) #define RS (PP1 + BIT3) #define D0 (PP2 + BIT1) #define D1 (PP2 + BIT2) #define D2 (PP2 + BIT3) #define D3 (PP2 + BIT4) //#define BACKLIGHT (PP1 + BIT0) // Commands #define CLEAR 0x01 /*****************************************************************/ /********* LOCAL FUNCTIONS *********/ /*****************************************************************/ void lcdDirPinout(unsigned int pin) { if(pin < P1orP2lcd){ P1DIR |= (pin & 0x00FF); }else{ P2DIR |= (pin & 0x00FF); } } /* * */ void lcdSetPinout(unsigned int pin) { if(pin < P1orP2lcd){ P1OUT |= (pin & 0x00FF); }else{ P2OUT |= (pin & 0x00FF); } } void lcdClrPinout(unsigned int pin) { if(pin < P1orP2lcd){ P1OUT &= ~(pin & 0x00FF); }else{ P2OUT &= ~(pin & 0x00FF); } } void lcdSetValue(unsigned char value) { if(value & 0x08){ lcdSetPinout(D3); }else{ lcdClrPinout(D3); } if(value & 0x04){ lcdSetPinout(D2); }else{ lcdClrPinout(D2); } if(value & 0x02){ lcdSetPinout(D1); }else{ lcdClrPinout(D1); } if(value & 0x01){ lcdSetPinout(D0); }else{ lcdClrPinout(D0); } delay_us(10); } void lcdTriggerEN() { lcdSetPinout(EN); delay_us(10); lcdClrPinout(EN); delay_us(10); } void lcdWriteData(unsigned char data) { lcdSetPinout(RS); // Set RS to Data lcdSetValue(data >> 4); // Upper nibble lcdTriggerEN(); lcdSetValue(data); // Lower nibble lcdTriggerEN(); delay_us(50); // Delay > 47 us } void lcdWriteCmd(unsigned char cmd) { lcdClrPinout(RS); // Set RS to Cmd lcdSetValue(cmd >> 4); // Upper nibble lcdTriggerEN(); lcdSetValue(cmd); // Lower nibble lcdTriggerEN(); delay_ms(5); // Delay > 1.5ms } /*****************************************************************/ /********* GLOBAL FUNCTIONS *********/ /*****************************************************************/ /* * */ void LCD_PortConfig(void) { // Direction lcdDirPinout(D0); lcdDirPinout(D1); lcdDirPinout(D2); lcdDirPinout(D3); lcdDirPinout(EN); lcdDirPinout(RS); } /* * */ void LCD_Initialize(void) { delay_ms(100); P2OUT = 0x03; // Start LCD (send 0x03) lcdTriggerEN(); // Send 0x03 3 times at 5ms then 100 us delay_ms(5); lcdTriggerEN(); delay_ms(5); lcdTriggerEN(); delay_ms(5); P2OUT = 0x02; // Switch to 4-bit mode lcdTriggerEN(); delay_ms(5); lcdWriteCmd(0x28); // 4-bit, 2 line, 5x8 lcdWriteCmd(0x08); // Instruction Flow lcdWriteCmd(0x01); // Clear LCD lcdWriteCmd(0x06); // Auto-Increment lcdWriteCmd(0x0C); // Display On, No blink } void LCD_SetText(char* text, int x, int y){ unsigned int i; if (x < 16) { x |= 0x80; // Set LCD for first line write switch (y){ case 1: x |= 0x40; // Set LCD for second line write break; case 2: x |= 0x60; // Set LCD for first line write reverse break; case 3: x |= 0x20; // Set LCD for second line write reverse break; } lcdWriteCmd(x); } i = 0; while (text[i] != '\0') { lcdWriteData(text[i]); i++; } } void LCD_SetInt(int val, int x, int y) { char number_string[16]; sprintf(number_string, "%d", val); // Convert the integer to character string LCD_SetText(number_string, x, y); } void LCD_Clear() { lcdWriteCmd(CLEAR); } void LCD_SetCharacter(unsigned char index, const unsigned char bitmap[8]){ unsigned short iter; lcdWriteCmd(0x38); lcdWriteCmd(0x40|(index <<3) & 0x3f); for (iter = 0; iter!=8;++iter){ lcdWriteData(bitmap[iter]); } lcdWriteCmd(0x02); } /*****************************************************************/ /********* END *********/ /*****************************************************************/
/*-----------------------------------------------------------------------*/ /* Low level disk I/O module skeleton for Petit FatFs (C)ChaN, 2009 */ /*-----------------------------------------------------------------------*/ #include <msp430.h> #include <stdint.h> #include "diskio.h" #include "pff.h" //#include "print.h" #include "spi.h" #define DELAY_100US() __delay_cycles(1600) // ( 100us/(1/16Mhz) ) = 1600 ticks #define SELECT() P2OUT &= ~BIT0 /* CS = L */ #define DESELECT() P2OUT |= BIT0 /* CS = H */ #define MMC_SEL !(P2OUT & BIT0) /* CS status (true:CS == L) */ void SoftSerial_xmit(uint8_t); #define FORWARD(d) SoftSerial_xmit(d) /* Data forwarding function (Console out in this example) */ /* Definitions for MMC/SDC command */ #define CMD0 (0x40+0) /* GO_IDLE_STATE */ #define CMD1 (0x40+1) /* SEND_OP_COND (MMC) */ #define ACMD41 (0xC0+41) /* SEND_OP_COND (SDC) */ #define CMD8 (0x40+8) /* SEND_IF_COND */ #define CMD16 (0x40+16) /* SET_BLOCKLEN */ #define CMD17 (0x40+17) /* READ_SINGLE_BLOCK */ #define CMD24 (0x40+24) /* WRITE_BLOCK */ #define CMD55 (0x40+55) /* APP_CMD */ #define CMD58 (0x40+58) /* READ_OCR */ /* Card type flags (CardType) */ #define CT_MMC 0x01 /* MMC ver 3 */ #define CT_SD1 0x02 /* SD ver 1 */ #define CT_SD2 0x04 /* SD ver 2 */ #define CT_BLOCK 0x08 /* Block addressing */ static BYTE CardType; /*-----------------------------------------------------------------------*/ /* Send a command packet to MMC */ /*-----------------------------------------------------------------------*/ static BYTE send_cmd ( BYTE cmd, /* 1st byte (Start + Index) */ DWORD arg /* Argument (32 bits) */ ) { BYTE n, res; if (cmd & 0x80) { /* ACMD<n> is the command sequense of CMD55-CMD<n> */ cmd &= 0x7F; res = send_cmd(CMD55, 0); if (res > 1) return res; } /* Select the card */ DESELECT(); spi_receive(); SELECT(); spi_receive(); /* Send a command packet */ spi_send((BYTE)cmd); /* Start + Command index */ spi_send((BYTE)(arg >> 24)); /* Argument[31..24] */ spi_send((BYTE)(arg >> 16)); /* Argument[23..16] */ spi_send((BYTE)(arg >> 8)); /* Argument[15..8] */ spi_send((BYTE)arg); /* Argument[7..0] */ n = 0x01; /* Dummy CRC + Stop */ if (cmd == CMD0) n = 0x95; /* Valid CRC for CMD0(0) */ if (cmd == CMD8) n = 0x87; /* Valid CRC for CMD8(0x1AA) */ spi_send(n); /* Receive a command response */ n = 10; /* Wait for a valid response in timeout of 10 attempts */ do { res = spi_receive(); } while ((res & 0x80) && --n); return res; /* Return with the response value */ } /*-----------------------------------------------------------------------*/ /* Initialize Disk Drive */ /*-----------------------------------------------------------------------*/ DSTATUS disk_initialize (void) { BYTE n, cmd, ty, ocr[4]; UINT tmr; #if _USE_WRITE if (CardType && MMC_SEL) disk_writep(0, 0); /* Finalize write process if it is in progress */ #endif spi_set_divisor(SPI_250kHz); DESELECT(); for (n = 10; n; n--) spi_receive(); /* 80 dummy clocks with CS=H */ ty = 0; if (send_cmd(CMD0, 0) == 1) { /* Enter Idle state */ if (send_cmd(CMD8, 0x1AA) == 1) { /* SDv2 */ for (n = 0; n < 4; n++) ocr[n] = spi_receive(); /* Get trailing return value of R7 resp */ if (ocr[2] == 0x01 && ocr[3] == 0xAA) { /* The card can work at vdd range of 2.7-3.6V */ for (tmr = 10000; tmr && send_cmd(ACMD41, 1UL << 30); tmr--) DELAY_100US(); /* Wait for leaving idle state (ACMD41 with HCS bit) */ if (tmr && send_cmd(CMD58, 0) == 0) { /* Check CCS bit in the OCR */ for (n = 0; n < 4; n++) ocr[n] = spi_receive(); ty = (ocr[0] & 0x40) ? CT_SD2 | CT_BLOCK : CT_SD2; /* SDv2 (HC or SC) */ } } } else { /* SDv1 or MMCv3 */ if (send_cmd(ACMD41, 0) <= 1) { ty = CT_SD1; cmd = ACMD41; /* SDv1 */ } else { ty = CT_MMC; cmd = CMD1; /* MMCv3 */ } for (tmr = 10000; tmr && send_cmd(cmd, 0); tmr--) DELAY_100US(); /* Wait for leaving idle state */ if (!tmr || send_cmd(CMD16, 512) != 0) /* Set R/W block length to 512 */ ty = 0; } } CardType = ty; spi_set_divisor(SPI_DEF_SPEED); DESELECT(); spi_receive(); return ty ? 0 : STA_NOINIT; } /*-----------------------------------------------------------------------*/ /* Read partial sector */ /*-----------------------------------------------------------------------*/ DRESULT disk_readp ( BYTE *buff, /* Pointer to the read buffer (NULL:Read bytes are forwarded to the stream) */ DWORD lba, /* Sector number (LBA) */ WORD ofs, /* Byte offset to read from (0..511) */ WORD cnt /* Number of bytes to read (ofs + cnt mus be <= 512) */ ) { DRESULT res; BYTE rc; WORD bc; if (!(CardType & CT_BLOCK)) lba *= 512; /* Convert to byte address if needed */ res = RES_ERROR; if (send_cmd(CMD17, lba) == 0) { /* READ_SINGLE_BLOCK */ bc = 40000; do { /* Wait for data packet */ rc = spi_receive(); } while (rc == 0xFF && --bc); if (rc == 0xFE) { /* A data packet arrived */ bc = 514 - ofs - cnt; /* Skip leading bytes */ if (ofs) { do spi_receive(); while (--ofs); } /* Receive a part of the sector */ if (buff) { /* Store data to the memory */ do { *buff++ = spi_receive(); } while (--cnt); } else { /* Forward data to the outgoing stream (depends on the project) */ do { FORWARD(spi_receive()); } while (--cnt); } /* Skip trailing bytes and CRC */ do spi_receive(); while (--bc); res = RES_OK; } } DESELECT(); spi_receive(); return res; } /*-----------------------------------------------------------------------*/ /* Write partial sector */ /*-----------------------------------------------------------------------*/ #if _USE_WRITE DRESULT disk_writep ( const BYTE *buff, /* Pointer to the bytes to be written (NULL:Initiate/Finalize sector write) */ DWORD sa /* Number of bytes to send, Sector number (LBA) or zero */ ) { DRESULT res; WORD bc; static WORD wc; res = RES_ERROR; if (buff) { /* Send data bytes */ bc = (WORD)sa; while (bc && wc) { /* Send data bytes to the card */ spi_send(*buff++); wc--; bc--; } res = RES_OK; } else { if (sa) { /* Initiate sector write process */ if (!(CardType & CT_BLOCK)) sa *= 512; /* Convert to byte address if needed */ if (send_cmd(CMD24, sa) == 0) { /* WRITE_SINGLE_BLOCK */ spi_send(0xFF); spi_send(0xFE); /* Data block header */ wc = 512; /* Set byte counter */ res = RES_OK; } } else { /* Finalize sector write process */ bc = wc + 2; while (bc--) spi_send(0); /* Fill left bytes and CRC with zeros */ if ((spi_receive() & 0x1F) == 0x05) { /* Receive data resp and wait for end of write process in timeout of 500ms */ for (bc = 5000; spi_receive() != 0xFF && bc; bc--) DELAY_100US(); /* Wait ready */ if (bc) res = RES_OK; } DESELECT(); spi_receive(); } } return res; } #endif