I am having a hard time using the bsl on my 5529 launchpad. I have modified the launchpad so that there is a usb cable that is connected to DM and DP on the MSP430 instead of the emulator that is normally connected to the DM and DP pins. This is so that I can test out a method for production programming of the processor.
When I press and hold the BSL pushbutton switch and plug in the USB cable to a PC in order to power things up I do see a USB device show up in the PC's device manager. I get a windows balloon that pops up and says 'USB device not recognized', and the device shows up in the USB controllers section as 'unknown device'. I have tried to load the driver for it named 'MSP430_CDC.inf' but it does not seem to work.
Has anyone else come across this type of behavior? Any suggestions? What should I expect to see when I plug in the USB cable to power up? I'm guessing that as long as I see it being classified as an 'unknown device' I will not be able to communicate via the BSL.
Thanks