When I change stack size in CCS Linker option (from default 80 to 120), I can see --stack_size is changed from 80 to 120 in the linker command line. However, the size of .stack section is always 0x40(dec 64). So why it is not consistent with --stack_size?
I have another project, where they are consistent. I don't why. Please help. Thanks
CCS Version: 6.0.0.00190
MSP430G2755
Compiler: TI v4.3.1