Hello,
we have 18.432 MHz crystal connected to the pins XOUT and XIN (port P7) of the microcontroller MSP430F5419. There are capacitors of 33 pF on both side of crystal connected to ground. There is 0.3 V only on XOUT. It seems to us it is too low voltage and therefore the microcontroller is so susceptible to electromagnetic interference.
We was trying to change the capacitance of capacitors near crystal and there is maximum amplitude (0.3 V) for 33 pF on XOUT. We have also changed the crystal to 7.3728 MHz and the problem is the same. We have also the boards with MSP430F149 and there it is ok - the voltage amplitude is more then 2V.
We also tried all combinations of XT1DRIVE in UCSCTL6 register and the voltage amplitude was the best (0.35V) for XT1DRIVE = 01 - it means the range from 8 to 16 MHz - but the crystal was 18.432 MHz.
Could you give us some advice how to increase the voltage amplitude on XOUT? Or is the amplitude of 0.3V normal for MSP430F5419?
Best regards,
Jiri Babka