Hi,
In my hobby weather station I use an MSP-EXP430F5529LP powered from the boosterpack connectors.
Now I'd like to start using an MT9D111 camera for capturing still photos but the voltage on the camera's interface cannot exceed 3.1V, ideally 2.8V. Instead of having a voltage translator for dozen of communication lines I'd rather lower the MCU's Vcc from 3.3V to 2.8V.
The question is whether I should expect any issues with LaunchPad components and MCU itself when lowered the voltage to 2.8V?
The datasheet is clear that the MSP430F5529 can be supplied with voltage of 1.8-3.6V so the only problem might be whether there are any 3.3V-dependent components on the LaunchPad.
Best Regards,
tml