I have an MSP430F5310 project that uses MSP430ware version 1.80.01.03. I checked the project into revision control and then checked it out on another PC. I did not check the MSP430ware directory into revision control as it is provided by TI as a resource.
However, on the second PC, I had MSP430ware 1.60.01.11 and 1.60.02.09. When I imported the project, CCS reported a warning "This project contains unresolved buildable linked resources".
I did not realize at the time that I had any MSP430ware installed so I went to Help->Install New Software and selected MSP430ware. CCS informed me that MSP430ware was already installed and that it was switching to an "Update" (rather than New Install I suppose).
So, CCS installed 1.95.00.32 but my project was using 1.80.01.03. We have a policy here that all developer MUST be able to build the exact same .hex file. So, just using the newest is not always an option, especially on a quick patch or short schedule.
So, now I have the following version installed:
1.60.01.11
1.60.02.09
1.95.00.32
So, how can I get CCS to install an intermediate (previous) version (1.80.01.03 in this case)?
Regards,
Jim