I'm using SmartRF05EB+CC2530 as transmitter and SmartRF05EB+CC2531 Dongle as receiver along with CC Debugger connected to SmartRF05EB+CC2531 Dongle.As a software i"m using SmartRF Studio7 through which i transmitted the packets between the 2 boards.Now i want to do packet sniffing/capturing using Smart RF Packet Sniffer software.How can I do this??
I"ve tried this in d following way
1)Receiver Side:Register export of RF Settings Template
2)saved that exported file with ".prs" extension
3)open Packet sniffer tool and select IEEE802.15.4/Zigbee2007
4)in the menu bar File->open data->select the ".prs"file which we saved in step2
5)as capturing device we select SmartRF05EB+CC2531
6)we get a set of packets here whose image below:
In d above image the rssi value which we observe while transmitting the packets in smartrf studio7 is not getting matched whn im exporting it and the fcs is showing as eror and the beacon payload whatever is shown is not understood
When i click on the play button to start capturing the packets I'm getting an error of Connect to EB smartRF05Eb is not selected connect to EB device failed:SmartRF05EB
how can i overcome this??
n also help me out by a correct way of using Packet Sniffering??
another question----
While exporting registers do we need to export the packet sniffer settings file in template??
If yes I'm not getting that file in my template list..try to help here also..