Hi,
I am trying to run Grace sample code "ADC12 TempSens Convert" on CCSv6 (Grace Ver3).
The device is MSP430F2618.
If I change the grace setting for ADC12 to use Timer_B7 Channel 1 as the trigger source
I get error saying 'timerLink' is sealed as shown below.
I get this error even if the Timer_B7 peripheral is enabled.
But I won't get the error if I select Timer_B7 Channel 0.
Is the Timer_B7 Channel 1 not supported?
Best Regards.