Hi,
I am facing following problems
1. The debugger does not go inside the " while (ADC12BUSY & ADC12CTL1 == 1) " at all. I do not know why? Plus the debugger shows me the correct value in Register " ADC12MEM0" but does not show the correct value of variable "SavedADC12MEM0".
2. I want to send the ADC sampled values to Tera Terminal. I can communicate with tera terminal well but unable to see the decimal values of the samples.
Melissa
My code is as follows
void Port_Init();
void adc_init(void);
void adc_start_Read(void);
void acc_read_with_offset();
void UART(int , int);
volatile int SavedADC12MEM0, SavedADC12MEM1 ;
unsigned int adc_index = 0;
//extern unsigned int SavedADC12MEM0[];
int main(void)
{
WDTCTL = WDTPW+WDTHOLD;
Port_Init();
while (1)
{
adc_init();
adc_start_Read();
// UART();
}
}
void Port_Init(void)
{
P3SEL = 0x30; // P3.4,5 = USCI_A0 TXD/RXD
P6SEL |= 0x80;
P6DIR |= 0x00;
P1DIR |= 0x01;
}
void adc_init(void)
{
REFCTL0 &= ~REFVSEL_3; //Page 693 of data sheet
REFCTL0 |= REFVSEL_2 + REFON; // Configure internal 2.5V reference
__delay_cycles(1900); // delay for reference to settle
ADC12CTL0 &= ~ADC12ENC; // Ensure ENC is clear
ADC12CTL0 |= ADC12ON | ADC12SHT0_15 | ADC12MSC ;//| ADC12REFON | ADC12REF2_5V;
ADC12CTL1 |= ADC12SHP | ADC12CONSEQ_2 |ADC12SSEL_0;
ADC12CTL2 = ADC12RES_2;
ADC12MCTL0 |= ADC12SREF_1 | ADC12INCH_7;
ADC12MCTL1 = ADC12SREF_1 | ADC12EOS;
__delay_cycles(1900);
}
void adc_start_Read(void)
{
REFCTL0 &= ~REFVSEL_3; //Page 693 of data sheet
REFCTL0 |= REFVSEL_2 + REFON; // Configure internal 2.5V reference
__delay_cycles(1900); // delay for reference to settle
ADC12CTL0 &= ~ADC12ENC; // Ensure ENC is clear
ADC12CTL0 |= ADC12ON | ADC12SHT0_15 ;//| ADC12REFON | ADC12REF2_5V;| ADC12MSC_0
ADC12CTL1 |= ADC12SHP | ADC12CONSEQ_1 |ADC12SSEL_0;
ADC12CTL2 = ADC12RES_2;
ADC12MCTL0 |= ADC12SREF_1 | ADC12INCH_7;
ADC12MCTL1 = ADC12SREF_1 | ADC12EOS;
__delay_cycles(1900);
P1DIR |= 0x01;
P1OUT = (uint8_t) (ADC12CTL1 & ADC12BUSY);
for(;;)
{
ADC12CTL0 |= ADC12ENC | ADC12SC;
while (ADC12BUSY & ADC12CTL1 == 0)
{
P1DIR |= 0x01;
P1OUT ^= 0x00;
SavedADC12MEM0 = ADC12MEM0;
SavedADC12MEM1 = ADC12MEM1;
}
SavedADC12MEM0 = 1234;
UART(SavedADC12MEM0, ADC12MEM1);
}
}
void UART(int a , int b)
{
volatile int buffer;
UCA0CTL1 |= UCSWRST; // **Put state matchine in reset**
UCA0CTL1 |= UCSSEL_3; // SMCLK
UCA0BR0 = 6; // 1MHz 9600 (see User's Guide)
UCA0BR1 = 0; // 1MHz 9600
UCA0MCTL = UCBRS_0 + UCBRF_13 + UCOS16; // Modln UCBRSx=0, UCBRFx=0,
// over sampling
UCA0CTL1 &= ~UCSWRST; // **Initialize USCI state machine**
UCA0IE |= UCRXIE; // Enable USCI_A0 RX interrupt
UCA0CTL1 &= ~UCSWRST; // **Initialize USCI state machine**
UCA0IE |= UCRXIE; // Enable USCI_A0 RX interrupt
buffer = a;
while (!(UCA0IFG&UCTXIFG)); // USCI_A0 TX buffer ready?
UCA0TXBUF = buffer; // TX -> RXed character
}
void adc_start_Read(void)
{
REFCTL0 &= ~REFVSEL_3; //Page 693 of data sheet
REFCTL0 |= REFVSEL_2 + REFON; // Configure internal 2.5V reference
__delay_cycles(1900); // delay for reference to settle
ADC12CTL0 &= ~ADC12ENC; // Ensure ENC is clear
ADC12CTL0 |= ADC12ON | ADC12SHT0_15 ;//| ADC12REFON | ADC12REF2_5V;| ADC12MSC_0
ADC12CTL1 |= ADC12SHP | ADC12CONSEQ_1 |ADC12SSEL_0;
ADC12CTL2 = ADC12RES_2;
ADC12MCTL0 |= ADC12SREF_1 | ADC12INCH_7;
ADC12MCTL1 = ADC12SREF_1 | ADC12EOS;
__delay_cycles(1900);
P1DIR |= 0x01;
P1OUT = (uint8_t) (ADC12CTL1 & ADC12BUSY);
for(;;)
{
ADC12CTL0 |= ADC12ENC | ADC12SC;
while (ADC12BUSY & ADC12CTL1 == 0)
{
P1DIR |= 0x01;
P1OUT ^= 0x00;
SavedADC12MEM0 = ADC12MEM0;
SavedADC12MEM1 = ADC12MEM1;
}
SavedADC12MEM0 = 1234;
UART(SavedADC12MEM0, ADC12MEM1);
}
}
void UART(int a , int b)
{
volatile int buffer;
UCA0CTL1 |= UCSWRST; // **Put state matchine in reset**
UCA0CTL1 |= UCSSEL_3; // SMCLK
UCA0BR0 = 6; // 1MHz 9600 (see User's Guide)
UCA0BR1 = 0; // 1MHz 9600
UCA0MCTL = UCBRS_0 + UCBRF_13 + UCOS16; // Modln UCBRSx=0, UCBRFx=0,
// over sampling
UCA0CTL1 &= ~UCSWRST; // **Initialize USCI state machine**
UCA0IE |= UCRXIE; // Enable USCI_A0 RX interrupt
UCA0CTL1 &= ~UCSWRST; // **Initialize USCI state machine**
UCA0IE |= UCRXIE; // Enable USCI_A0 RX interrupt
buffer = a;while (!(UCA0IFG&UCTXIFG)); // USCI_A0 TX buffer ready?
UCA0TXBUF = buffer; // TX -> RXed character
}