Hi i am using msp430f2410 MCU with CCS 6.0 compiler.
32KHZ external clock is connected to Xin/Xout (Pin8&9)
Below is my code.
#include "msp430f2410.h" void main(void) { WDTCTL = WDTPW + WDTHOLD; // Stop Watchdog Timer if (CALBC1_8MHZ ==0xFF || CALDCO_8MHZ == 0xFF) { while(1); // If calibration constants erased // do not load, trap CPU!! } BCSCTL1 = CALBC1_8MHZ; // Set DCO to 8MHz DCOCTL = CALDCO_8MHZ; P5DIR |= 0x70; // P5.6,5,4 outputs P5SEL |= 0x70; // P5.6,5,4 options while(1) { } }
When i run this program the program execution stops inside the for loop.
I want to know why it is stopping there and how to resolve this issue?
Thanks in Advance,
Vinoth