What is FLL in MSp 430 need details.... How it works and what is the hardware for FLL. How it is different from PLL.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What is FLL in MSp 430 need details.... How it works and what is the hardware for FLL. How it is different from PLL.
FLL = Frequency Locked Loop
PLL = Phase Locked Loop
I am unable to find more details about FLL. can you please send me some link on FLL (detailed info - not one paragraph.)I do not need any more information or tutorial About PLL.
Somnath Pradhan said:No tutorial needed about PLL
Very good. FLL measures frequency error (higher/lower freq), PLL measures phase error (ahead/behind phase). The remaining parts of both are more or less equal - error signal is used to steer VCO (voltage controlled oscillator) or DCO (digitally controlled oscillator).
Somnath Pradhan said:Is it possible to implement FLL in DSP.
Indeed. You measure both - oscillator frequency and reference frequency, compare them. Then passing error signal through loop filter steer your oscillator ( VCO or DCO or even DDS ).
Possibly not the best articles, but at least I did what you asked: used google for you.
https://www.eecis.udel.edu/~mills/ntp/html/discipline.html
http://www.semtech.com/images/datasheet/xe8000_tn_09_locked_loop.pdf
seems to be information..... i have found some iEEE paper on this http://ieeexplore.ieee.org/xpl/login.jsp?tp=&arnumber=938354&url=http%3A%2F%2Fieeexplore.ieee.org%2Fiel5%2F82%2F20317%2F00938354.pdf%3Farnumber%3D938354
hope this will help
Basically, an FLL compares two frequencies by counting the clock pulses of the target frequency during one clock pulse of the reference frequency, and comparing the count with the given factor. Then it raises or lowers the target frequency in fixed steps. For a long-time average, this is fine. And doesn’t require much energy (after all, it is just two counters and a compare). But it limits the possible target frequencies to an integer multiple of the reference.
The reference clock can be very low, which reduces the power required for a low-frequency crystal, with a high factor. (you can get 25MHz from a 32kHz reference). In fact, the higher the factor, the better the result (less long-time jitter due to constant corections). FLL fails if the factor is too low, and for best results it should be >32 due to the 32 modulation steps in the DCO.
A PLL requires a lot of power, as it compares the phase of the target frequency and the phase of the source frequency, based on multipliers and dividers. When locked, a PLL gives an accurate (not average) output frequency that is not necessarily an integer multiple of the reference. The required reference frequency must be fairly high, with a low factor, because the lock precision depends on frequent updates (or the output frequencfy may 'jump'). The PLL used for MSP430-USB builds 48MHz from a reference that is at least 1.5MHz (4MHz when using a crystal).
**Attention** This is a public forum