In my project, I would like to alter the .out file in the postprocessing step (some configuration data which is generated externally is to be written into the file). I have successfully converted the .out to .txt and patched that one, but I have no real idea how to convert it back to .out.
When I try to flash the .txt file (whose formatting etc. is ok, I checked with a diff tool), the MSP430 seems to idle around somewhere in the 0xFExx range, I cannot reset it via the debugger. So using the .txt file is not an option at this point in time. As far as I can tell, the programming step itself is ok, I did a copuple of cross checks between debugger and .txt file.
Does someone have a suggestion how to either modify the .out or get the MSP running with the .txt file?
Max