Hi,
I've used CCS to download simpleUsbBackchannel (in MSP430Ware) on my MSP-EXP430F5529LP. It runs fine.
Now I want to change the UART port from USCI_A1 module to USCI_A0. So I need to do these change if soruce code:
- All "UCA1_x" change to "UCA0_x" in BCUart.h and BCUart.c.
- P4.4 (TXD) and P4.5 (RXD) change to P3.3 and P3.4 in BCUart.c, respectively.
- P6.7 (RTS) and P1.7 (CTS) change to P2.6 and P2.3, respectively.
But I can not find the P6.7 and P1.7 in these (main.c, BCUart.h and BCUart.c.) files. Where can I find them?