Hi,
I am sorry to ask the same question...
With respect to MSP430F5521 I would like to know what could happend to the
device if we use 0.1uF instead of 400nF as per the datasheet?
One of our customer has unfortunately designed their product
with 0.1uF capacitor connected to the VCORE pin on MSP430F5521.
But after 3000 hours of usage, one device had a problem on ADC input port and
was returned back for failure analysis.
We came to know that few of the I/O ports are damaged on this MSP430.
So, we would like to know if the improper capacitor connected to VCORE pin
could cause such problem and damage the I/O ports in a long run.
This information is very helpful for us to judge if we should stop the mass production
and re-design the board again.
Best Regards.
kummi