I am working on a project that requires custom bootloader software and custom application software on a MSP430G2553. I have completed the application software and tested it. I am still working on the bootloader software. I am using MSPGCC running under linux. Is there a way when I compile to software to specify the addresses that the two pieces of code are programmed at? For example the bootloader for be programmed in to the MSP starting at address 0xC000 and I wish to program the application code beginning at address 0xCA00. So how would I tell the compiler that my application code starts at address 0xCA00 instead of the default 0xC000?