I'm developing a Java application that connects to TI's BSL and loads firmware images. Invoking via the TEST+RESET sequence was not simple but I'm now able to put the MCU into BSL with the use of a simple FTDI converter. Writing and reading the target flash is quite easy once the MCU is running on BSL.
Now the problem comes when I want to reset the MCU to make it run the user application. Bringing RESET to low for a while does not work for some reason. I've also tried to use multiple combinations of RESET + TEST levels without success. slau319i just says that RESET has to be tied to low and then switched back to high whilst TEST is kept high in order to reset the MCU but this is not working.
Any suggestion about how to quit the BSL and start the custom application with a true hardware reset?
Thanks.