Hi!
I'm not sure if this is the right form for my question about power supply.
I've been using ADS1231REF module as basic weigh-scale system for my Raspberry pi project. It sends data to a cloud where they are analyzed and displayed.
http://www.ti.com/tool/ADS1231REF?keyMatch=ads1231ref
To apply power to the ADS1x31REF, I plugged in a 6V–9V ac wall adapter.
Unfortunatly my ac adapter has a replaceable tip/sleeve. And by accident I left a reversed power source connected for longer than a few seconds.
From datasheet:
AC adapters must be tip positive/sleeve negative. When an ac adapter is plugged in, the board always
takes power from it, and not from the battery.The ADS1x31REF is protected against polarity reversal. If a power source is connected in reverse by mistake, the display remains blank. To prevent damage to the board, do not leave a reversed power source connected for longer than a few seconds.
Best regards
Boris