Hey,
First of all I'm new in using MSP430. I bought the TRF7960A EVM, which is a development board that contains RFID and a MSP430F2370.
The board has a JTAG connector and I'm trying to program it using a MSP-FET430UIF. I tried to burn this board, an also a home made board. The programs that I used was the CCS and the FET-MSP. It was impossible to burn it and I always get the same feedback.
FET-MSP:
=====================================
Reading Code File ........................... done
-- Code size = 0x0000 ( 0 ) bytes
JTAG communication initialization.... failed
Verifying Security Fuse .................... failed
--------------- FAILED !!! -----------------
CSS:
I know that is a typical problem, and I can understand that maybe I have a short circuit in my own board. But the TRF7960EVM is working and is a company device, so I should be able to program it.
Any of you have an Idea how can I solve it?
Thanks!