I am writing a series of very simple application using the MSP430G2553 launch pad to drive the signal channels of some of our latest PCB and to gather information from them. This way, we can avoid to build complicated testers using switches, et.
I have already done three of them and they are being used successfully in our production facilities.
I decided to use the Energia feature of CCS6.0 and see how practical it would be for this kind of application. All went very well until I decided to use the SPI library. The task is to communicate with an AD7798. However, even when I see the AD7798 responding back to the launch pad, the return from the SPI.transfer() routine call is always 0xFF.
I can write the same program using a more conventional C program but it bothers me that I cannot get this one to run.
Maybe it is something I am overlooking, so any suggestions would be helpful please.
Thank you...-ANDY