Good Morning all,
I am Vinod Naik....I am very much new to Microcontrollers and MSP430. I know a little bit about MSP430 launchpad.
I would like to implement a wireless sensor network to monitor the temperature. The wireless sensor network consists of two nodes and a gateway.
The two nodes are built around MSP430G2553. For each node a temperature sensor(DHT11) and an RFtransceiver(nRF24L01) interfaced to it. Each node has to sense the temperature and need to transmit it to the the Gateway.
The Gateway is also need to be built around MSP430G2553 and this has to be connected a PC(computer) for the monitoring the temperature received from the two nodes. The Gateway is also interfaced to RFtransceiver(nRF24L01) again.
The nodes have to sense the temperature and need to send the data to the gateway every 1 minute, and the gateway has to receive this data from the two nodes and need to display on the computer screen.
I request you to help me in doing this. And I need to complete this within 25 days. Please provide me the links for implementing the above said project. I am ready to discussion also. my email id is vinodrathode@gmail.com and contact no +919704584984