Hi,
I've lately been having trouble with programming my custom target board (based on MSP430F6736) using my MSP-FET. The MSP430F5529LP on-board debugger successfully programs the board 100% of the time! But, with the MSP-FET, I get one success in about 100 tries!
The message I get is:
MSP430: Trouble Writing Memory Block at 0x4000 on Page 0 of Length 0xd60: Could not erase device memory
MSP430: File Loader: Verification failed: Target failed to write 0x04000
MSP430: GEL: File: <programName>.out: Load failed.
Can anybody offer any suggestions?
I should clarify that it is externally powered in both instances.