I've recently run into an issue on one particular msp430f248, out of several production devices, that halts when I set the DCO using the 1MHz cal values. I've inspected/captured the InfoA ROM and it's values look reasonable 0x86(BCSCTL1) and 0xDA(D0CTL).
If I single step the assembly the JTAG session dies when D0CTL is written. It looks like the clock stops altogether, and I can't get it back until I reset the processor.
Has anyone else seen this? Do i just have a bad proc?
Thanks