hi
i am working on a project with msp430f2274, using its ADC in order to monitor the temperature conditions. i want to use the channel 12 in order to take the input for ADC but its not working properly for this channels. for other channels i.e from 0- 8 its working properly.Do anybody no the reason behind it or i can't monitor the analogue signals from the channel 12 ?