CCS 6.0.1.00040, MSP430G2755. In Project -> Properties -> Build -> MSP430 Linker -> File Search Path, added "libmath.a" to the top of ' Include library file ... as input ' and "${CCS_BASE_ROOT}/MSP430/lib/5xx_6xx_FRxx" to the ' library search path '. If I ' #include <msp430_math> ' I get the error ' #1965 cannot open source file "msp430_math" ' plus the warning ' #10204-D: could not resolve index library "libmath.a" to a compatible library '; if I ' #include<math.h> ' I just get the warning. The output format is eabi (ELF).
Thanks,
Doug