I can't find it now, but I've read somewhere in the TI literature that if the WDT is not to be used as the clock for ADC, it must be turned off. Is that correct?
I'm using the WDT as an interval timer, clocked by the 8 MHz SMCLK divided by 32768, and I don't want to stop it. But about 4 times a second, I want to do an ADC clocked by something much faster. Is there a problem doing that? Seems like there shouldn't be.