If I want to use pin 9 as the ADC input, which of the following do I need to do?
1. Select 0111 for INCHx in ADC10CTL1
2. Set bit 7 in ADC10AE0
3. Set bit 7 in P1SEL
I assume the first two, but in sample code I usually don't see the third. But maybe that's because it's assumed that's done elsewhere, or maybe it's because doing the second one means the P1SEL value doesn't matter. Anyway, I would appreciate clarification on this.