Dear all,
I need to capture the USB traffic in a USB communication. I want to capture the traffic on the bus in high impedance so that I do not affect the communications between master and slave.
After that, I need some device (a microcontroller with a built-in USB) which listens to USB frames and decode them for me so that I get the payload of all USB traffic.
The problem is that the USB of the microcontroller will not be host/slave of any device since it will listen the signals in high impedance (with a high impedance differential amplifier). Thus I need that the USB can be configured in promiscuous mode. That means, listening everything and send it up to the driver.
Is that possible with some microcontroller of TI portfolio?
Many thanks in advance.
Regards,
Jorge.