Hi,
I am using MSP430F5325 for my project. I have few queries.
1. Does internal RTC runs on DVCC or AVCC.
2. Apart from manual reset on reset pin/watchdog reset,Is there a Software reset command to reset the controller.
3. While RTC is running ,on provide software Reset command will the RTC current value ill be retained and continue to tic or lost.
4.If my controller is in LPM03 and the voltage drops below 2.2V(Below Wake up voltage) will the RTC module run?
Looking forward for reply
Best regards,
Sunil H S