Good day,
I'm asking if someone has trying succesfuLly the example in the SLAA450C with the MSP430G2XXX at the end of the text, I have two issues.
1. When I send the SYNC character from host to device 0xBA, actually reads 0x72h, IT looks like the lost of two bits.
2. I don't know how to use the hex2bin, I can find de hex file.
As you can see I'm a newvie in BSL matters, and I would like to check the viability of the example, I'm working with IAR 5.4
REGARDS.
ANDRÉS FELIPE RODRÍGUEZ