I tried to connect 3.3V External Battery to the MSP432P401R Launchpad to the Pins (3.3v / Gnd) on the Right of the board - it did not work. However, when I connected the same 3.3v (external battery) to the 5V and Gnd on the Left of the board, the board started running. I have been running it for 2 hours, it is running steady? Is this the right connection for an external supply. By the way, both Jumpers for 3V and 5V are set. Any suggestions?