Hello,
Starting a new design and I am in trouble with uC selection. I don't know what device should I chose. The project primary goal is data acquisition over SPI using ADS1256. For high channel count I am planning to use 4 ADS1256 (16Channel) The right sampling speed for ADC is 500SpS with 32pga value. I would like to stream the data to PC over uart. ( Not planning to use USB)
I think the bottleneck is the uC to PC transmission. 4times of 500Sps is a large amount of data, and I am doubt that the F5529 is able to handle it. Thats why I am taking account the new MSP432
The reason why I choose F5529 is I have experience with that device, large community background.
However the MSP432 has many useful features and parameters like floating point support or higher cpu speed and so on. Relatively new design.
What is your recommendation? When and why do you suggest MSP432 instead of MSP432?