I am using MSP430F5529 experimenters board which act as a SPI slave in MODE 0 (data toggled on falling edge and sampled at rising edge of clock). I have enabled both TX and RX interrupts for UCB state machine. SPI is working in 4 pin mode.
So I am able to do some transaction through the SPI but after some time, the data is not shifted out from the MSP slave properly , i can see a bit shifting in the SOMI line,,(probed using DSO). what might be causing this issue after successfull operation for some time ??