Using MSP430FR5969 Launchpad, TI-RTOS 2.12 and CCS 6.1.
I would rather use an external 32.7kHz crystal oscillator for timing instead of the internal crystal for better accuracy, but when I probe the 2 pins of the external crystal, there is no signal on the scope, just noise. Am I probing incorrectly, or do you need to set register(s) to enable the external crystal?
I tried the below code (to set the pin multiplex mode to crystal instead of GPIO) but it just threw the board into a bootloop:
PJSEL1 &= ~BIT4;
PJSEL0 |= BIT4;
CSCTL4 &= ~LFXTBYPASS;
Is there anything you need to do in the config to set the RTOS timers module, etc to use the external crystal?