I have just downloaded the latest version of CCS V6.1 and am having problem compiling my code.
I have a simple project and have used Grace to configure a MSP430FR5849 device.
However when I compile the code I get the following errors:
symbol in file
--------- ----------------
__TI_cleanup_ptr C:\ti\ccsv6\tools\compiler\ti-cgt-msp430_4.4.4\lib\rts430x_lc_rd_eabi.lib<exit.obj>
__TI_dtors_ptr C:\ti\ccsv6\tools\compiler\ti-cgt-msp430_4.4.4\lib\rts430x_lc_rd_eabi.lib<exit.obj>
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "TamperDetection_V4.XX MSP430FR5849.out" not built
Now if I disable the MSP430 MPU option in the Project Options menu I do not get this error and my code compiles without a problem.
Can any one please give me a clue as to why this is happening?
Thanks.