Hi community member,
Please let me confirm the following question.
[Question]
In my understanding, if the MCLK is operating faster than 8 MHz, wait states are required to ensure reliable FRAM access. When using MCLK ≥ 8 MHz, configure the FRAM wait states in software before configuring the MCLK frequency. Thus, we need to add as below.
FRCTL0 = FRCTLPW | NWAITS_1;
In case of using the grace for initialize with 16MHz, does this setting add to init code automatically?
* We used the Grace, it seems that this settings did not add for initialize of device code.
Best regards.
Kaka