Hello ,
i have a msp432 launchpad and i need to design some embedded systems with msp432.
they need to be programmed with pc by other users like arduino.so i need to help.
1.jtag programmers are expensive and people need to pay programmer circuit. like old times.
2. msp432 launchpad have a xds110-et debugger/programmer interface. it's so nice but i don't want it on the board. because it's big and complex. and getting really hot. i don't like it.
3. i need to bsl for the msp432. actually i was worked with bootloaders before(pic bootloaders). but i don't get it how to use in msp432. do you have any schematic , software or videos ? i have a ft232 pc-uart,level converter and other circuits. i just don't get it how to use it.
now i am tring to BSL_Scripter.exe but it is not working.
how i can burn to bootloader to msp432 ?
BSL_Scripter command line output is :
Initializing, Mode: P4xx UART 115200 COM12 DONE
Mass Erase: Fail(0x51)
Like that. if i was press the reset button on the launchpad , first line is "done", but if i don't , it's gonna writing 'fail'.
if i connect ft232.dtr pin to msp432launchpad.rst pin. it's fail too. and it always resetting the msp432.
sorry for my english is maybe bad. thanks.
Cevat