Hi,
If external crystal(32.768kHz) is not there then what is the impact on the system. In our project we are using MSP430F5659 controller for NFC.
Kindly provide me with your suggestions.
Thank you,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
If external crystal(32.768kHz) is not there then what is the impact on the system. In our project we are using MSP430F5659 controller for NFC.
Kindly provide me with your suggestions.
Thank you,
Selva,
Have a look in the user's guide, chapter 5 Unified Clock System (page 158 and following).
Dennis
Hi Dennis,
I gone through that document, but i'm not able to conclude for the above query.
Regards,
Selva
What exaclty do you mean with "not there"? Does your hardware have a crystal, and you want to know what happens when it fails? Or do you want to build hardware that works both with and without a crystal?
Hi Dennis,
I have gone through that.
But I need to know that if I use only internal clock(32.768khz) and don't use external clock, how will the Timers viz,..MCLK, ACLK and SMCLK work or will they not work as expected?
Also, whether current consumption changes if we have a system without external crystal(32.768khz)?
Hi Selva,
if you don' have an external crystal present, you could use the REFO instead. That is a built in oscillator that is meant as a substitute in case you can't or don't want to use an external crystal.
It is not as accurate as an external watch crystal and needs a bit more supply current but you can save the costs for the crystal.
If you don't necessarily need the 32.768kHz, you could use a different internal clock as source for the ACLK, for example the VLO (typ. 9.4kHz) which is having a lower accuracy and higher spread but needs significantly less current.
Thanks and best regards,
Christoph
**Attention** This is a public forum