I am needing to connect multiple (of the same) device to a USB bus at once. I have read that I can manually assign a serial number to each of the devices when flashing the program. I would like to be able to recognize which serial number has been connected to the USB bus and which port it was assigned to on my windows machine. If you have any information on how I can manually assign a serial number 1-8 to my devices so that when connected I can keep track of them in the C# gui that would be very helpful.
Thanks in advance,
Kellen