I am using MSPFlasher application version 1.03.07.00 on Linux. I am running an automated hardware in the loop system with multiple programmers so I require use of the "-i" option to specify connection port.
It does not handle the -i option correctly (i.e. "-i /dev/ttyACM3").
Doing some quick debug it appears there are two issues:
1) The passed argument is capitalized at some point which causes an issue when compared against "ttyACM".
2) After I hacked #1 I found another problem. Per the documentation the argument should be passed in the form "/dev/ttyACM0", but it only seems to work for "ttyACM0".
Hoping these issues can be addressed in the next release.
Thanks.