I’d like to setup so that the main clock runs from an external 24Mhz source on XIN pin. I write CSCTL2 register to 0x0000 to select MCLK to XT1CLK. I set CSCLT3 to 0x0000 so everything is divide by 1. CSCT4 to 0xC1F0 to set XT1 Source from external clock in high frequency mode. PJSEL1 to 0x30 to set enable the XIN/XOUT functions. This doesn’t work so what more am I missing? I’ve a feeling I’m violating a configuration rule that I’m not aware of or I’m missing an enable somewhere.