Hi,
I am working with the MSP432 and one of the ADC examples from the driverlib. The microcontroller started running fine for a while, then sporadically overheating and I get this error in CCS:
CORTEX_M4_0: JTAG Communication Error: (Error -261 @ 0x0) Invalid response was received from the XDS110. (Emulation package 6.0.14.5)
CORTEX_M4_0: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging.
There's nothing much to the circuit- a ~1.1V signal into an analog input and ground into ground. The signal is generated from three double A batteries passing through a voltage divider. The same setup has been used on an MSP430 for over a year with no issue, so I don't think it has anything to do with that.
If I unplug the device, let it cool, then try again it usually works for a while then happens again. Any advice?
Thanks,
Becky